STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM1 6pwm how to disable - STM32F427

Posted on November 22, 2017 at 21:10The original post was too long to process during our migration. Please click on the attachment to read the original post.

Bogdan by Senior
  • 2233 Views
  • 3 replies
  • 0 kudos

Resolved! L1 cache for stm32H743

Posted on November 20, 2017 at 20:53Dear all,I am trying to set-up a new board using an stm32H743.In my tests, I initialized the MPU in order to use the cache L1 with the Flash.When I initialize the MPU to use the cache, the results are really impre...

AT Commands are not working (NUCLEO-L152RE)

Posted on November 16, 2017 at 15:18HiI am trying to get details by using AT Commands (AT, AT+GMR, AT+CWLAP, and etc) but i am getting the same command which i am sending through Serial write.Example: If I send basic command as �AT\r\n�, I need to g...

Putting STM32F437xG into Standby mode more than once

Posted on November 22, 2017 at 12:46I have some code which puts my STM32F437xG into Standby and wakes it up on RTC.  In my test code this works fine: I can go into Standby for, say, 10 seconds (enabling just the battery-backed RAM, flash is off), re...

Beginner need help: Wakeup from STOP-Mode

Posted on November 21, 2017 at 18:51Hello everybody,I would be happy if someone could help me. I am very new with STM32 controllers and i have problemes to understand the wakeup function from the STOP-Mode with the external interrupt.I have search a...

Zh4ng Wu by Associate
  • 1145 Views
  • 2 replies
  • 0 kudos

Modbus library for STM32F2

Posted on November 14, 2017 at 07:24Hi I am looking for Opensource modbus library for STM32F207 processor.I found freeModbus but it needs to be ported on STM32F207.Is there any other modbus library available?Has anyone already ported freeModbus libr...

How to set the max buffer size for DMA in STM32L4?

Posted on November 21, 2017 at 23:24I am trying to collect data using ADC + DMA continuous mode. I aim to get 2400 data points using DMA. The code is based on the one generated using STM32CubeMx. The data I got from my PC using UART were just 2048 p...

Current in Low power mode for STM32H7

Posted on November 22, 2017 at 11:58Dear All,I'm using STM32H743 Nucleo board.I want verify power consumption. Specially in low power mode.When I flash the micro with PWR_STOP_RTC project (in stm32Cube exemple), i have 10ma  in low power modeI measu...

aneveux by Associate II
  • 705 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.