STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

help httpserver on nucleo board: I pay for it

Posted on November 22, 2017 at 10:23HiI am late in y project and need some help with a HTTP server.This is what I need:a webserver for FW download which also gives me the opportunity to change IP Address and Netmask, ideal on a nucleo stmf429zi boar...

I2S3 48KHz16bit Extended data format issue

Posted on November 22, 2017 at 03:17I am trying to configure I2S3 in Fullduplex Master RX mode, 48KHz sample rate. Hal Configuration is as shown belowhAudioFDI2s.Init.AudioFreq = AudioFreq; hAudioFDI2s.Init.ClockSource = I2S_CLOCK_PLL; hAudioFDI2s.I...

Is this a bug in cubemx?

Posted on November 18, 2017 at 09:37 generate code project ====> The initialization function actually inside the main function。

0690X0000060PFdQAM.png 0690X0000060PDHQA2.png
one V by Associate III
  • 874 Views
  • 2 replies
  • 0 kudos

Setting up MPU for External SRAM + NOR + SDRAM

Posted on November 21, 2017 at 03:39I am working on a project based of stm32f746G EVAL board. It uses LCD controller with frame buffer in SDRAM, internal flash for code, external flash to store fonts and media, and external SRAM for RW+ZI data. Fina...

Disable interrupts

Posted on November 21, 2017 at 05:47STMF4 is running and using some of the interrupts.A a new piece of code needs to be protected from all interrupts but a specific one, which has the highest priority in this application.The trivial solution: Go thr...

isaac by Associate II
  • 2692 Views
  • 3 replies
  • 0 kudos

sample code of stm32 to initialize LCD(newhaven display)

Posted on October 29, 2015 at 22:47 I have been using LCD (glass on chip) made by newhaven display for a while. They provided sample code to initialize. However the code is mostly for microchip, not for STM32 hal drive. Some people have been s...

rwmao by Senior
  • 6288 Views
  • 5 replies
  • 0 kudos

STM32 I2C Only transmit address

Posted on November 21, 2017 at 20:54dear All,what is the probable reason of HAL_I2C_Master_Transmit() transmits only address?regards,Rasool#i2c #stm32f4 #master-trasnmitter

rsharifi9 by Associate III
  • 1094 Views
  • 1 replies
  • 0 kudos

In what order are registers pushed into the stack after the exception occurs?

Posted on November 21, 2017 at 19:24In Cortex M3, what is the order in which the register are pushed into the stack?Which of the following orders are correct (if any)?First Order:      PC      PSRx      R3      R2      R1      R0      R12      Link ...

VBAT ADC voltage measurement incorrect at low voltages

Posted on November 21, 2017 at 20:52Hello,I have a problem with VBAT voltage measurement on a STM32F401VB.As can be seen in the picture below, the ADC output is correct (identical to the calculated value ''ADC Should'') in the upper region of the in...

0690X0000060PFwQAM.png
Fr4nky by Associate II
  • 811 Views
  • 0 replies
  • 0 kudos

ADC measuring

Posted on November 21, 2017 at 20:47Hello!I want to calculate battery voltage, that connected to STM32L476RG board.I've connected ADC pin and this battery with divider (so Vbattery<Vref.adc).But I need to know how to get some factors/parameters.See ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.