STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ARM Math library for STM32L4 ?

Posted on November 23, 2017 at 14:13Dear All,Is it possible to used Arm math library for FFT calcul on STM32L4 cible ?Because, I can compile, but when lunch programm, I go in this error loop :Thanks

0690X00000608spQAA.png
aneveux by Associate II
  • 875 Views
  • 0 replies
  • 0 kudos

Resolved! How to declare a big arraw in User RAM with STM32H743ZI

Posted on November 23, 2017 at 11:31Dear all,I'm using STM32H743ZI (nucleo-H743ZI board)This µc have 1Mb of SRAM (512 Kbytes of user sram ?)When i declare array of 100k uint16I have this error message :'section `.bss' will not fit in region `DTCMRAM...

aneveux by Associate II
  • 1436 Views
  • 2 replies
  • 0 kudos

Problems with the ADC/DAC

Posted on November 22, 2017 at 11:45Hello:I�m using my STM32L432 to input a signal from the Signal Generator and I�m trying to get the same signal, after using the ADC and DAC (photo below)Here is the program I write, but it doesn�t work. Could some...

0690X0000060PEMQA2.jpg 0690X00000604AyQAI.jpg 0690X0000060PFYQA2.jpg

I2S interface issue on STM32F7 Nucleo board

Posted on November 23, 2017 at 13:15Hi.,I am working on STM32F767ZI Nucleo board, In this I am trying to interface external audio board through I2S interface, I configured I2S in Master receive mode using STM cubeMX, But I am not able to receive any...

bug in STM32 LWIP in IAP example?

Posted on September 07, 2017 at 08:07could it be that in STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAPthe latest firefox is not supported?FW download via internet explorer works but but not firefox 55.0.3 (32-Bit) !Thx

STM32F7

Posted on November 23, 2017 at 11:17Hello all; i want to display data on the LCD-TFT of  STM32F746G using the Arduino IDE can you help me?Thanks.

STM32 PMSM FOC LIB seminar

Posted on November 22, 2017 at 17:47Is there a webinar or a seminar somewhere to get start with the motor control library?#motor-control-foc-library #sdk-foc #foc-sdk-4.3.0

STM32F407 DMA Transfer Peripheral to Peripheral

Posted on November 19, 2015 at 18:32 Hello, I'm wondering if it is possible like with the pic32 to initiate a DMA transfer from peripheral to peripheral. So far the documentation I've read specifies periph to memory, memory to periph, or mem...

Configure USB Bulk IN/OUT packet size 256 bytes

Posted on November 21, 2017 at 03:52Hello, I'm the STM32F207 user, as title mentioned, I have a trouble when configure the usb packet size from the default 64 bytes to 256 bytes. The problem is that my usb device may not be able to connect with all ...

calvin by Associate III
  • 10280 Views
  • 4 replies
  • 0 kudos

Dfuse demo v3.0.6 release ?

Posted on November 23, 2017 at 01:27Hi.I've posted articles about dfuse in the past.https://community.st.com/0D50X00009XkYMSSA3 The answer is v3.0.6 is said to have been modified.'I had this same issue and ST gave me a Pre-Release version of the DFU...

Jin ho An by Associate II
  • 1918 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.