2017-11-22 3:46 AM
I have some code which puts my STM32F437xG into Standby and wakes it up on RTC. In my test code this works fine: I can go into Standby for, say, 10 seconds (enabling just the battery-backed RAM, flash is off), return at reset, go back into Standby, wake up 10 seconds later, and repeat ad infinitum.
I have now integrated this code into my main application and I find that I can go into Standby successfully but, once I have returned from Standby, I can no longer go back into Standby successfully again; something is waking me up immediately, returning at the reset vector, rather than waiting for the RTC alarm I have set to wake up.
I have checked that, when I attempt to go back into Standby, no interrupts other than RTC are enabled, the PWR_CR_CWUF flag is cleared and the previous RTC alarm has been reset with:
RTC->ISR &= ~RTC_ISR_ALRAF;
RTC->WPR = 0xCA;
RTC->WPR = 0x53; RTC->CR &= ~RTC_CR_ALRAE; RTC->WPR = 0xFF; EXTI->PR = RTC_EXTI_LINE_ALARM_EVENT;What else could be causing the MCU to wake up again immediately? How can I find out what's causing the wake-up? FYI, battery backed SRAM is being maintained correctly and none of the RCC flags (RCC_FLAG_PORRST, RCC_FLAG_SFTRST, RCC_FLAG_IWDGRST, RCC_FLAG_PINRST, RCC_FLAG_LPWRRST) are set on return from reset.
Rob
2017-11-22 8:53 AM
Fixed it! I was being an idiot: my sleep time was in seconds my sleep function takes milliseconds. Everywhere else I was multiplying by 1000, just not in this one case. Nice to have a simple one...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.