2017-11-21 2:24 PM
I am trying to collect data using ADC + DMA continuous mode. I aim to get 2400 data points using DMA. The code is based on the one generated using STM32CubeMx. The data I got from my PC using UART were just 2048 points. I guess I need to change the max buffer size of the DMA. I try to set the CNDTR register in the initialization, but it was not successful. I guess the location could be wrong, or there are other codes required.
I am new to the STM32 family. I hope someone can help me address it. I also attached all my codes.
// partial codes.
//This is the function in main.c.
HAL_ADC_Start_DMA(&hadc1,(uint32_t*)adcValue,2400);
//DMA initialization (Partial)
:
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{/* ADC1 DMA Init */
/* ADC1 Init */ hdma_adc1.Instance = DMA1_Channel1; hdma_adc1.Init.Request = DMA_REQUEST_0; hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE; hdma_adc1.Init.MemInc = DMA_MINC_ENABLE; hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_adc1.Init.Mode = DMA_CIRCULAR; hdma_adc1.Init.Priority = DMA_PRIORITY_LOW; hdma_adc1.Instance->CNDTR = DataLength; // I was trying to change the buffer size here, but it did work. if (HAL_DMA_Init(&hdma_adc1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
}
Thanks in advance.
Hailing
#buffer-size #stm32l4-hal #dma-stm322017-11-21 3:40 PM
What is BUFSIZ and where is it defined?
JW
2017-11-21 5:05 PM
Hi JW,
By saying 'Buffer Size', I mean the 'DMA channel x number of data register (DMA_CNDTRx) (x = 1..7,
where x = channel number)'. This is mentioned in the reference manual for STM32L4. I guess this register controls the number of data transmitted using ADC+DMA.I also have a macro called 'BUF_SIZE' defined in the beginning of main.c. It sets the number of data points from each adc channel.
Thanks for your reply. Regards,
Hailing
2017-11-21 5:26 PM
By BUFSIZ I mean BUFSIZ, as in HAL_UART_Transmit(&huart1,(uint8_t*)datastore1,BUFSIZ,2000) etc.
JW
2017-11-21 5:33 PM
Sorry, that should be BUF_SIZE.
HAL_UART_Transmit(&huart1,(uint8_t*)datastore1,BUF_SIZE,2000);
Hailing
2017-11-21 5:37 PM
OK so you changed the sources. What are the symptoms now?
JW
2017-11-21 5:48 PM
I am not in my office now. I will test it tomorrow morning and let you know. Thanks for your kindly help.
Do you think the way I set the buffer size is correct (CNDTR)? As I remember, when I tested the code in the debug mode. The points I got in each array(datastore1,2,3,4) were 512. The rest in the array are zero.
Anyway, I will try tomorrow.
best regards,
Hailing
2017-11-21 5:50 PM
Do you think the way I set the buffer size is correct (CNDTR)?
No. In Cube/HAL, CNDTR is set when you start the transfer. Read the Cube documentation, or sources if documentation is not sufficient.
JW
PS. BUFSIZ is a standard macro from <stdint.h>, see C99 7.19.1.
2017-11-22 4:05 AM
Hi JW,
Thanks for your help. I changed the variable from BUFSIZ to BUF_SIZE. It turns out to be my mistake. I can now transfer 8000 points without setting the CNDTR register.
Thanks,
Hailing
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.