STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

timer prescaler triggers on first rising edge

Posted on January 22, 2018 at 10:28 Hey everyone, I'm using a stm32f722ze I've got a small issue considering the prescaler on the timers. I'm using this to trigger an input capture and DMA request after 8 clock cycles, although the prescaler se...

con3 by Senior
  • 3441 Views
  • 8 replies
  • 0 kudos

unable to update Options bytes

Posted on October 27, 2017 at 23:32Hi All, I am trying reprogram my board- MCU-STM32F405RGT6, programmer/debugger: ST-Link/V2. It says read protection activated (when I check my options byte REAd protection is set to level 1 ). I try to change the r...

Reema O by Associate II
  • 2281 Views
  • 9 replies
  • 0 kudos

Resolved! STM32F303ZE Why is my SPI3 module transmitting 16-bits

Posted on January 22, 2018 at 16:44I have my SPI3 module configured as a master.  I want it to transmit 8-bit words.  Here is my setup as read from the chip while its executing.  No matter what I do each time I write to SPI3->DR it transmits 16-bits...

0690X00000609PjQAI.png
a b by Associate
  • 1433 Views
  • 4 replies
  • 0 kudos

how can i implement 3 I2C buses on a STM32 LO family. Although it has 3 these are split across AF6 and AF7 alternative pin mapping ?

Posted on January 22, 2018 at 14:39how can i implement 3 I2C buses on a STM32 LO family.looking at the data sheet for pin mapping this are mapped in to PB & PA buseswith alternative Mode does not allow all 3 to be expossed, as these are spread acros...

STEVAL-STLKT01V1 Sensor Tile connect to I2C device

Posted on January 21, 2018 at 21:54I have a STEVAL-STLKT01V1 Sensor Tile. I want to add additional sensing capabilities and was wondering how to add a peripheral that communicates over I2C? Are there any firmware examples of how to do this?#stm32l4-...

stm32H743 and usart2 problem

Posted on November 29, 2017 at 17:26Dear All,I have just ported the RTOS uKOS (http://www.ukos.ch) on the new stm32H743. Everything work fine at the exception of the usart2. I have strange situations with the interruptions, and as soon as I receive ...

Analog watchdog is not firing more than once

Posted on January 19, 2018 at 17:21Hi,i want to use the analog watchdog (ADC) on my STM32F4. I have an analog sensor attached to channel 1 of ADC1. I dont want to use CPU to make constant function calls to ADC, even with ADC interrupt mode i have to...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.