STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA with ADC Injected mode/stm32f4

Posted on January 19, 2018 at 15:52hello, I'm working with the stm32f4-discovery Board , in fact i have a problem using the DMA with an ADC 'injected channel'. I've configured the DMA to transfer the converted data from the injected data register 'J...

stm32cubemx V4.23.0 bug report.

Posted on December 18, 2017 at 07:18when used the 103 series MCU,  the SWD port will been disabled in follow step.1) enable the SWD interface. 2) enable tim3 CH1 PWM function and remapping the output pin to PB4. 3) when the tim3 init code run to __H...

Bruno Hu by Associate II
  • 1340 Views
  • 2 replies
  • 0 kudos

IAP jump to APP, but it don't work.HELP!!!

Posted on January 17, 2018 at 11:38Hi,I was doing IAP&App in STM32F030rc. When I finish IAP and APP, and run from IAP to jump to APP, it can not be realized. I have try many ways, but useless. Please help me, I have waste a lot of time for this func...

Resolved! Error[Li005]: no definition for ''HAL_CRC_Init''

Posted on January 23, 2018 at 02:24I want to add crc function in STM32F030RC, so I add HAL_CRC_Init, and related functions. But there is always 'no definition for 'HAL_CRC_Init'' error when link. I have include 'stm32f0xx_hal.h','stm32f0xx_hal_crc.h...

STM32F0 let IAP jump to APP1 or APP2

Posted on January 22, 2018 at 04:39I want to realize a OTA function that IAP jump to APP1 or APP2. But I have a doubt whether need I to generate two APPs for OTA, because the APP1 and APP2's vecotor is different(If my customer has done lots of OTA, ...

emWin GUIBuilder not working for STM32F746 Discovery?

Posted on January 16, 2018 at 17:38I am using the STemWin GUIBuilder for STM32F429 Discovery and this works fine. Trying the same procedure with the STM32F746 Discovery causes partial distortion on the screen. For example Slider and Buttons have a l...

''Can not connect to target'' using ST link utility

Posted on March 22, 2017 at 13:22'Can not connect to target'error message popup appears,when i am trying connect target.I am using St link utility.can some one help me out.I am using STM32l017K8 Microcontroller.and also i am using SWD interface to p...

reading I/O register values with command line GDB

Posted on December 18, 2017 at 16:54Recently I found that STM32CubeMX support Makefile as well as SW4STM32. So far I worked with only the SW4STM32, but now I'm happy to move to the command line development with GCC, GNU make , stlink, and GDB. After...

M. Jeong by Associate II
  • 5481 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.