STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BSP LIBRARY IAR WORKBENCH STM32F303VC

Posted on January 22, 2018 at 14:00Good evening,I can't  import BSP library in IAR Workbench. I'm using stm32f303vc board and I'm followed this guide but i have always the same problem(https://community.st.com/docs/DOC-1500-how-to-add-a-bsp-on-top-o...

Symon by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

I2C to AT24C64

Posted on February 08, 2017 at 10:35i want to using External EEPROM via I2C on STM32F051R8T6.but i always get error when compile it.can someone tell me or help me ?

noval by Associate II
  • 4306 Views
  • 8 replies
  • 0 kudos

[SOLVED] How to set up a GPIO interrupt on STM32L031

Posted on January 21, 2018 at 14:02Please can somebody point me to an example of setting up an interrupt and service routine for a GPIO input for an STM32L031? I have read UM1749 but it maybe it's because I'm not familiar with HAL (4 years of using ...

sm23 by Associate II
  • 5043 Views
  • 7 replies
  • 0 kudos

I2S (in SPI): I2SDIV [7:0] = 1

Posted on January 22, 2018 at 10:57In RMs for 'F4/'F7/'F0 (I didn't check further), in SPIx_I2S prescaler register (SPIx_I2SPR) chapter, I2SDIV description, the following statement is given:I2SDIV [7:0] = 0 or I2SDIV [7:0] = 1 are forbidden values.H...

0690X00000609AUQAY.png

Maximum Timeout for Window Watchdog(WWDG)

Posted on January 18, 2018 at 06:44I have a question regarding the WWDG in STM32F103RB. What can be the maximum timeout using the WWDG or even better question will be what will be the optimum value of the APB1 clock period(ms).I know the Maximum va...

Stm32l4 iir compute time

Posted on January 20, 2018 at 20:48Hello engineers,I would like to ask you about your computing time of your iir. Ive tried cmsis but ive measured avg. 50us computing time for 32 samples using direct form biquad single stage filter. Many thanks for ...

marek2399 by Associate II
  • 1693 Views
  • 3 replies
  • 0 kudos

STM32f4 USB HS HAL Driver bugs

Posted on April 19, 2017 at 23:28Hello.I'm working on application of USB communication with high speed (about 50 Mbit/s). So I used ULPI PHY.For some purpose I used CubeMX (v 4.20.1) and was surprising that my application didn't work.  Enabling DMA ...

STM32F303vc discovery import BSP library in IAR

Posted on January 21, 2018 at 19:54Hi,I have some problems with import the BSP library in IAR Workbench. I'm using stm32f303vc discovery board and i want to use the gyroscope and accelerometer installed on the board. I also followed this guide (http...

Symon by Associate II
  • 1032 Views
  • 0 replies
  • 0 kudos

Sending small amout of data in high frequency using usb

Posted on January 21, 2018 at 19:10hi every one, i am using STM32CUBE with STM32F4 processor and i want to send small amout of data through USB but it takes a long time using the CUBE function USB_CDC_TRANSMIT. can someone help me do, thanks!

Ita Dab by Associate
  • 760 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.