STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

flash example can't not run on STM32L4R5QG

Posted on March 15, 2018 at 12:10I have two customer boards as below :A board : Mount with STM32L4R5QII (2MB internal flash)B board : Mount with STM32L4R5QGI (1MB internal flash)A board run well on the STM32L4R5ZI-Nucleo\examples\flash many times.B ...

fema by Associate III
  • 2102 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L4 RTC

Posted on March 15, 2018 at 19:43Hi all,I'm facing an odd behavior working with an L4/Nucleo64/CubeMX/HAL. RTC peripheral. Same result w/ and w/o LSE oscillator.Basically, a code like this:while (1) {   HAL_RTC_GetTime(&hrtc, &sTime, FORMAT_BCD);   ...

Virtual Screen API on STM32F469I-DISCO

Posted on March 13, 2018 at 23:29Hi,I want to use the virtual screen API of STemWin on this board (using STM32Cube_FW_F4_V1.21.0).There is no special folder in the 'Projects'-Folder for the 'F'-board. Just 'STM32469I-Discovery'.Nevertheless, the sam...

Resolved! wake up from stop mode using I2C

Posted on March 15, 2018 at 14:05Hi everybody,i'm using STM32L051T6 MCU and i need to wake up from stop mode using I2Ci've read the last datasheet version and it is possible but there is an errata sheet that reports thati it is impossible.The datash...

Measuremet of internal temperature on ST32F303RCT6

Posted on March 13, 2018 at 18:46We have been using processor temperature measurement for a long time with different families of STM32: M3, F3, F4. Only the processor STM32F303RCT6 does not work. The measured voltage of the sensor is 2.22V and is re...

milan23 by Associate II
  • 3358 Views
  • 6 replies
  • 0 kudos

Resolved! stm32f071 - Port PD2 not configurable as output

Posted on March 15, 2018 at 18:34Dear everybody,in my code, i am not able to set my Port PD2 as output.As can be seen, I stopped debug at line 294.In lines 287 and 289 GPIOD->MODER and memory adress 0x4800 0C00 should be set to some value unequal ze...

0690X0000060A0zQAE.png

External loader in ST utility

Posted on March 15, 2018 at 17:16I am trying to create a custom external loader for the flash chip used in my product. I have looked the example projects in IAR and created myown. I modified the Loader_src.c and Dev_Inf.c file according to my flash ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.