cancel
Showing results for 
Search instead for 
Did you mean: 

Measuremet of internal temperature on ST32F303RCT6

milan23
Associate II
Posted on March 13, 2018 at 18:46

We have been using processor temperature measurement for a long time with different families of STM32: M3, F3, F4. Only the processor STM32F303RCT6 does not work. The measured voltage of the sensor is 2.22V and is relatively unstable (voltage for 25C is 1.43V). I just created a simple project that only measures the internal temperature sensor. This program works on STM32F303VCT6 but does not work on STM32F303RCT6. The conditions are exactly the same, 8MHz oscillator, 3.3V power supply. Other measurements in full application work normally. It seems like the internal temperature sensor is not connected to the internal input 16 of the ADC1 converter. Does anyone have a similar experience?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User
Posted on March 13, 2018 at 18:52

Do you use the appropriate sampling time; AVDD/AVSS connected correctly and decoupled; etc.?

This program works on STM32F303VCT6 but does not work on STM32F303RCT6.

What is the value of  DBGMCU_IDCODE (at 0xE004 2000) for both?

JW

Posted on March 14, 2018 at 15:25

STM32F303RCT6: 0xE0042000: 0x10036422

STM32F303VCT6: 0xE0042000: 0x10036422

I found another problem. On RCT6 is not working also Vrefint measurement on ADC1. ADC value is 4095 on ADC_Channel_Vrefint. On ADC2 Vrefint measurement is OK.

Best Regards,

Milan

________________

Attachments :

image001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxrB&d=%2Fa%2F0X0000000b1v%2FD3kZpw3.JhRRY4f8pOuY8vSnn15DuakS3rH0SKaQWeQ&asPdf=false
Posted on March 14, 2018 at 23:12

Except of what I've written above, I am out of ideas, sorry.

JW

Posted on March 15, 2018 at 10:40

Just to make sure: you checked that you do set TSEN and VREFEN properly for both ADCs - in the same register?

And have you tried to measure VBAT?

JW

Posted on March 15, 2018 at 17:17

The same program without any change is working on VCT6. TSEN and VREFEN are correctly set. We are using MCU several years in a lot of different projects without any problem. I try to use simple example project without any interrupts,…. . External crystal 8MHz is used. I also try to use internal, but it is fully the same:

/*

Posted on March 15, 2018 at 20:42

Then probably the only option is to ask ST for support.

JW

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.