2018-03-13 3:29 PM
Hi,
I want to use the virtual screen API of STemWin on this board (using STM32Cube_FW_F4_V1.21.0).
There is no special folder in the 'Projects'-Folder for the 'F'-board. Just 'STM32469I-Discovery'.
Nevertheless, the sample
STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Applications\STemWin\STemWin_HelloWorldcompiles, links, debugs and runs without problem.- Changes in LCDConf_stm32469i_discovery.c:
--------------------------------------------------------------#define NUM_BUFFERS 1 /* Number of multiple buffers to be used */
#define NUM_VSCREENS 2 /* Number of virtual screens to be used */- Changes in BASIC_HelloWorld.c: ---------------------------------------------#define DISP_X 800#define DISP_Y 480volatile int hx;
void MainTask(void) {
GUI_Clear(); GUI_SetFont(&GUI_Font20_1); GUI_DispStringAt('Virtual screen 1.4', DISP_X - 140, DISP_Y - 40); GUI_DispStringAt('Virtual screen 2.3', 20, DISP_Y + 20); GUI_SetOrg(0, DISP_Y); while(1) { hx++; }}Compiles, links, debugs without problem, but: The first screen keeps displayed!?
Any suggestions?
Harry
2018-03-15 2:33 PM
Well,
I got some further information. During initialization we have the call-tree and the result on the data of hltdc_disco.Instance:
- GUI_Init()
- GUI_Config() - LCD_X_Config() - LCD_LL_Init() - LTDC_Init(); - HAL_LTDC_Init(); -> hltdc_disco.Instance: seems to be valid - HAL_DSI_Start(&hdsi_disco); -> hltdc_disco.Instance: all zero !!!hltdc_disco.Instance keeps all zero on further processing...It is rather difficult to understand the neccessary steps to initialize the LCD, maybe someone could help... The DSI-locic seems to be the root cause...
Harry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.