2018-03-15 11:43 AM
Hi all,
I'm facing an odd behavior working with an L4/Nucleo64/CubeMX/HAL. RTC peripheral. Same result w/ and w/o LSE oscillator.
Basically, a code like this:
while (1) {
HAL_RTC_GetTime(&hrtc, &sTime, FORMAT_BCD);
HAL_RTC_GetDate(&hrtc, &sDate, FORMAT_BCD); printf('DateTime ......', ......, sTime.Hours, sTime.Minutes, sTime.Seconds);HAL_Delay(1000);
}
Results in:
DateTime - 1/1/2000-1-0:0:0
DateTime - 1/1/2000-1-0:0:1DateTime - 1/1/2000-1-0:0:2DateTime - 1/1/2000-1-0:0:3DateTime - 1/1/2000-1-0:0:4DateTime - 1/1/2000-1-0:0:5DateTime - 1/1/2000-1-0:0:6DateTime - 1/1/2000-1-0:0:7DateTime - 1/1/2000-1-0:0:8DateTime - 1/1/2000-1-0:0:9 DateTime - 1/1/2000-1-0:0:16DateTime - 1/1/2000-1-0:0:17DateTime - 1/1/2000-1-0:0:18DateTime - 1/1/2000-1-0:0:19DateTime - 1/1/2000-1-0:0:20DateTime - 1/1/2000-1-0:0:21DateTime - 1/1/2000-1-0:0:22DateTime - 1/1/2000-1-0:0:23DateTime - 1/1/2000-1-0:0:24DateTime - 1/1/2000-1-0:0:25DateTime - 1/1/2000-1-0:0:32...
DateTime - 1/1/2000-1-0:0:56
DateTime - 1/1/2000-1-0:0:57DateTime - 1/1/2000-1-0:0:64DateTime - 1/1/2000-1-0:0:65...
DateTime - 1/1/2000-1-0:0:88
DateTime - 1/1/2000-1-0:0:89DateTime - 1/1/2000-1-0:1:0DateTime - 1/1/2000-1-0:1:1So:
Any idea?
Solved! Go to Solution.
2018-03-15 2:41 PM
BCD means Binary Coded Decimal (more precisely it's packed BCD).
In BCD, you count
0x00, 0x01, 0x02... 0x09, 0x10, 0x11, 0x12... 0x58, 0x59, 0x00, 0x01...
But you then take those BCD numbers and print them in decimal, which for the same sequence as above is:
0, 1, 2... 9, 16, 17, 18... 88, 89, 0, 1....
and that's exactly what you observe.
JW
2018-03-15 2:41 PM
BCD means Binary Coded Decimal (more precisely it's packed BCD).
In BCD, you count
0x00, 0x01, 0x02... 0x09, 0x10, 0x11, 0x12... 0x58, 0x59, 0x00, 0x01...
But you then take those BCD numbers and print them in decimal, which for the same sequence as above is:
0, 1, 2... 9, 16, 17, 18... 88, 89, 0, 1....
and that's exactly what you observe.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.