STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32Fxxx ICT using JTAG

Posted on March 15, 2018 at 16:20To begin, this is a board TEST question rather than a design question: Has anyone successfully generated digital In-Circuit Test vectors for the STM32F4xx families using the Keysight 3070 or Teradyne scan tools? I su...

NUCLEO-H743ZI LWIP using STM32cubeMX?

Posted on November 06, 2017 at 11:11Hi,  I generated a simple LWIP/UDP project for the NUCLEO-H743ZI using the STM32cubeMX. But the function HAL_ETH_Transmit(&heth, &TxConfig, 0); returns with DMA error .  My board works using the example from the S...

Asantos by Senior
  • 1432 Views
  • 4 replies
  • 0 kudos

Reading variable length strings from a usart with DMA

Posted on October 05, 2017 at 22:44 I need to read variable length strings from a usart. The strings may be the result of local programming or not. I'm using the HAL DMA receive driver under FreeRTOS. I've found that the following approach works:...

Second I2C bus generating 60 Hz square wave at SCL

Posted on March 15, 2018 at 14:51I have successfully implemented an initial I2C bus (I2C1) in my custom board design (using STM32F405).  I then added a second I2C bus (I2C2) to my design and have initiated it and set it up identical to I2C1.  The fi...

Eric P by Associate
  • 888 Views
  • 1 replies
  • 0 kudos

f_getfree API returns FR_INVALID_DRIVE error

Posted on March 15, 2018 at 10:31Hi clive,I am using a 32 GB SD card,My code by using the API f_getfree() is as follows:if (f_mount(&myFATAFS, SDPath, 1) == FR_OK) {HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);f_getfree('1:', &Free_clust, &myFATAFS);tot_s...

SD card memory status checking

Posted on March 09, 2018 at 07:59Hi I am storing files into SD card using the SDIO interface. I am using a 32 GB sd card. Now i want to check everytime how much space is available on the sd  card. Are there any API's available to do this? I am using...

Can't access to thread from yesterday: Unauthorized

Posted on March 15, 2018 at 08:33Hi ST Team,I wrote yesterday in following thread but today I get no access?? Whats wrong?https://community.st.com/0D50X00009XkX4ZSAV#stm32forum #st-community #threads #unauthorized

H S by Associate III
  • 714 Views
  • 3 replies
  • 0 kudos

STM32L073VBT6 COST 100mA,Help

Posted on March 14, 2018 at 08:09My product with stm32l073vbt6 ran 1 week or longger,the mcu was broken.All io and peripheral on broken mcu can run as normal,But the power consumption up to 100mA not 100uA!I have removed all other part but mcu and s...

ren yong by Associate II
  • 6730 Views
  • 19 replies
  • 0 kudos

Wake from stop mode

Posted on March 15, 2018 at 08:06Hi,     I am using a STM32LO72 device and entering stop mode using     HAL_PRW_EnterSTOPMode ( PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);     I have configured the RTC AlarmB to wake the device but it wakes almost...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.