STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I try to configure the ADC of a STM32F407 to work in triple injected simultaneous mode, but only ADC1 works. How do I have to configure the ADC's that they work simultaneous?

As stated in the Reference manual. I configure the master ADC1 to get the trigger from the TIM2 TRGO and this ADC1 is working when started. ADC2 and ADC3 start only when I configure JEXTEN (=0x01) and JEXTSEL (=0x03) in CR2 of the according ADC. I do...

ATasc by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

Is it possible to get Vbus disconnect notification on self-powered USB HS device in STM32H743 without wiring VBus to an IEXT port?

I have a working USB2 (ULPI) device mode interface, and want to detect cable removal. There appears to be provision for this: OTG_GINTSTS has SRQINT and OTGINT bits and OTG_GOTGINT has the OTGINT bit, but I do not seem to get any response to cable r...

STM32F4 Timer Input capture problem

Posted on May 19, 2018 at 12:48Hello , I am using stm32f446re nucleo board . and i face some issue in timer input capture . here i am using 2 timers TIM6 ( for time base generation ) and TIM2 (free running input capture purpose)actually my code is w...

RN by Senior
  • 4115 Views
  • 10 replies
  • 0 kudos

STM32F722 - i2c data acquisition using timer interrupts

Hello,I'm having some trouble using the timer based interrupts.I have some very basic experience in mcu programing but I'm new to the STM32 platform and I had to adapt to it rather quickly. Therefore I lack some of the basic knowledge.My first questi...

0690X000006C8lBQAS.jpg
KMarci by Associate II
  • 962 Views
  • 0 replies
  • 0 kudos

Problem with form of SCK clock of SPI protocol !

I have been trying to perform SPI communication and observe outgoing and incoming data through MOSI & MISO. There is a weird problem in SCK weveform There are the codes I wrote :#include "stm32f10x.h" #include "stm32f10x_rcc.h" #include "stm32f10x_gp...

0690X000006C8kwQAC.png
KOzdi by Associate II
  • 2715 Views
  • 2 replies
  • 0 kudos

Can complementary timer pins be used as inputs?

Hello, I'm designing a PCB with an interface to an existing STM32769 board. I would like to use one of the STM32 timer inputs to trigger a timer. When the timer reaches its "compare" value it should trigger a DMA request for an SPI transaction. Accor...

AKuch.0 by Associate
  • 1206 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.