2018-10-08 1:20 AM
As stated in the Reference manual. I configure the master ADC1 to get the trigger from the TIM2 TRGO and this ADC1 is working when started. ADC2 and ADC3 start only when I configure JEXTEN (=0x01) and JEXTSEL (=0x03) in CR2 of the according ADC. I don't know howw to use the common trigger as stated in the reference manual:
"13.9.1 Injected simultaneous mode
This mode converts an injected group of channels. The external trigger source comes from
the injected group multiplexer of ADC1 (selected by the JEXTSEL[3:0] bits in the ADC1_CR2
register). A simultaneous trigger is provided to ADC2 and ADC3." from DocID018909 Rev 15
Thanks for your help in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.