STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EEPROM Read/Write STM32L15x

Hi,I am having a problem with using internal EEPROM memory for saving data. I can read data only from BASE adress of EEPROM. I can not write to EEPROM or read form any other place in EEPROM.MY simple code:#define FLASH_EEPROM_BASE ((uint32_t)(FLA...

JAN R by Associate III
  • 909 Views
  • 2 replies
  • 0 kudos

Program code.

Difficult and stupid question.There is an interrupt SVC_Handler written in assembly language. There are many internal addresses in the function body, which for convenience of use are collected in a table in the function header. The table is used to n...

Resolved! How to use TCM memory on the STM32F7 series?

I am working on FreeRTOS on the STM32F777II. Was just curious, how can I configure TCM (CCM) memory for use and how can I force the linker to use this TCM memory only for selected variables declarations?

QubeBox and lwIP

Hi,I want use LwIP, but i wan't use PPP. How to definitly remoove PPP from generated Makefile ?RegardsGrzegorz

Can't send TCP message exactly more than 1000 times

HiI'm using STM32F439 Dev Board and LWIP as TCP/IP stack; I'm using TCP echoserver example. the board is connected to PC. when I send a message from PCto the board, it echoes back the message. But there is a problem. aftersending exactly 1000 message...

HI i am trying to get the example project for interfacing USB stick into my custom board which has STM32F429II now , I could not find it in any of your latest Cubeprjects or anywhere in example projects,

I want to know how do i interface the USB stick to my board and start communicating with it.basically i want to read .bin/.png/.dfu files from USB stick Please provide the example project as soon as possible 

Vprabhu by Associate II
  • 922 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.