STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H5 PLL Nfract issue

Hello, I am using STM32H503 for precise time measurement hence I need to tune the PLL that output frequency compensates the voltage or temperature drift of the HSE crystal.My setup is:- Clock configured as HSE=16, M=, N=337, Nfrac=4096, P=2 which sho...

hijax_pl by Associate III
  • 1962 Views
  • 3 replies
  • 0 kudos

PyOCD Programming

Hello, I’m trying to use the PyOCD library to program an STM32H747 and an STM32U5A9 using .hex or .bin files generated by STM32CubeIDE. So far, I haven’t had much success, and I’d like to know if anyone has experience with this or can offer guidance ...

Resolved! Nucleo-303RE Not Starting Up

I am using a Nuclro-303RE to develop a USB Virtual Com port, and I am running into an issue that I cannot seem to resolve.  Just to verify things, I did put some really simple code in the flash the green indicator on the Nucleo board.I have it connec...

Nucleo-F303RE-Clock.png Nucleo-F303RE-USB.png Nucleo-F303RE-VCOM.png Bryon08_0-1744207627697.png
Bryon08 by Associate II
  • 3052 Views
  • 5 replies
  • 2 kudos

Using STMCubeIDE and Micropython

I want to add a USB thumb drive (mass storage) to a NUCLEO-144 F767ZI board. I see the STM32CubeIDE can be used to point GPIO lines PA8~PA12, PG6, PG7 to connector CN13 (USB Micro-AB) or to the Morpho connectors to realize a USB OTG (On the Go) inter...

Resolved! STM32F746ZG DFU MODE

HELLO guys could you please tell me how to put the stm32f746zg board in dfu mode actually earlier i was able to program and use the stlink to dump but currenty im not able to connect using stlink so i want to do with the dfu stm32 bootloader mode i h...

joyson by Associate
  • 2275 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.