STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N647 Maximum Pixel Through DCMIPP and ISP

Dear Community, I am researching how to use a 50Mpx MIPI CSI-2 2 LANE RAW 10 sensor with stm32N647.The idea is not to use the full sensor, instead using analogue/digital crop and windowing on the sensor to capture a specific part of the image and dow...

Resolved! Can't program/connect to STM32U031K4U6 over SWD

Hi all, I have reached the point of desperation, and I am all out of ideas how to get my STM32U031 project working.I designed a very simple PCB which has only a few components. I have attached the KiCad files in case it is helpful. I followed guideli...

Screenshot From 2026-04-03 02-41-12.png IMG_20260403_023607.jpg IMG_20260403_023614.jpg IMG_20260403_023347.jpg
EricNava by Associate III
  • 1017 Views
  • 13 replies
  • 1 kudos

STM32G070CBT6 IC pins shorted internally

Hi,I have made up six boards and three of them had an unusually high standby current (35mA instead of 1mA).Eventually, when the IC was removed, we found Pins 5 & 6 of the removed IC were shorted internally (0.3R)They were also shorted to pin 45 with ...

patrickreddesigns_0-1752670173666.png

Set up PWR_SMPS_1V8_SUPLLY_LDO STM32H755ZIT6

Dear al!i need your help, i design PCB use STM32H755ZIT6, i set up mode PWR_SMPS_1V8_SUPLLY_LDO via STM32CubeMX 6.12.1. I expect core M7's clock is 400Mhz, M4's clock is 200Mhz. I measure voltage after L2 is 1.8V, at each Vcap pin is 1.0V, The MCU wa...

Resolved! VDDCSI, VDD33USB pin on STM32N6

Hi,I do not plan to use USB or CSI, and the board only receives 1.8V power. So, I asked how to connect the VDD33USB pin, and I was told to just connect it to GND. However, I have two more questions.I currently have the VDDA18USB and VDDA18CSI pins co...

TIM7 is stopping after working

Hi everybody,I'm working on a STM32F446. I'm using the UART.I've a function with switch/cases which instead of a function number fill a buffer.ex :switch(function) {case 0x00 : Txbuffer[idx_trame++] = 0x00;break;case 0x01 : Txbuffer[idx_trame++] = 0x...

tim7.png
fab04 by Senior
  • 323 Views
  • 2 replies
  • 1 kudos

Beginner example for DCMIPP on STM32N6570DK

Hello, I wanna use the development board STM32N6570-DK for taking a picture with MB1854B. i am quite new for DCMI and DCMIPP. i just want to read the image through the pipe1 of dcmipp but i dont know how to config the MCU in .ioc file. Can anyone exp...

pawatJoy by Associate III
  • 577 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.