STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! About Ouput Compare Insert dead time .

Now , I generate below waveform. Every thing is OK except for red arrow , it indicate a deadtime.but it's longer than other deadtime , in fact , This dead time is twice as large as the other dead time .​divide into three stage :1�?First Stage , TIM r...

0690X00000986RLQAY.png

Problem with using external crystal oscillator

Hi Everyone,We are using the following code to generate clock pulse for STM32F722 from an external 12MHz crystal. However, whatever we do it sounds the STM32F722 gets its clock pulse from an internal 16 MHz oscillator. The reason for using an extern...

DHes by Associate II
  • 3929 Views
  • 7 replies
  • 0 kudos

How to store a text file in Nucleo?

I am using a Nucleo F429ZI. I have noticed when I plug it in via the debugger, my computer treats it like an external drive (which it calls NODE), where it seems I can store stuff. Is it possible to store a text file in this space generated from my p...

JChan.0 by Associate II
  • 1385 Views
  • 1 replies
  • 0 kudos

Trouble triggering TIM2 capture compare from TRC

Hi there, I'm using the STM32H7 and I need to get one of the SAI FS signals to go through a pre-scaler and trigger a capture compare on TIM2 CC3.The only solution for this seems to be to use SAI2_FS_A -> TIM5_ETR1 -> TIM5_TRGO -> TIM8_ITR3 -> TIM8_TR...

Mttjcksn by Associate III
  • 8112 Views
  • 5 replies
  • 0 kudos

SmBus Comm Problem

We need to Smbus Communication to use BQ78350(Texas Instrument) with STM32F051R8T6. We studied the example codes in your website. (https://www.st.com/en/embedded-software/x-cube-smbus.html) But the examples are so complicated to understand. We need t...

SIM900A GSM module with stm32f1

I'm trying to send message to sim900A via the serial port. The AT commands work but the GSM replies with some unwanted text (Previously sent text ) then finally OK. The GSM is supposed to reply what I typed with some prompts and finally OK. The pict...

0690X00000989dUQAQ.png
ASeyo by Associate II
  • 1223 Views
  • 0 replies
  • 0 kudos

What are the correct values for embedded flash wait state setting and programming delays for VOS0 range and AXI clock 240MHz?

Hi,I'm using a STM32H745 and looking at RM0399 rev 2. In table 15 for the flash memory timings there are no values for VOS0 range and the maximum frequency in the table is 225MHz. Going by other sections of the document the maximum Faclk is 240MHz.I ...

mickminn by Associate III
  • 1166 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.