cancel
Showing results for 
Search instead for 
Did you mean: 

Does the signal SAI2_FS_A not trigger when SAI 2 is in synchronous slave mode?

Mttjcksn
Associate III

Hi there,

I'm using the SAI2_FS_A signal to trigger a capture event on TIM2 (Through a series of weird internal routing). It all works nicely when SAI2 is an asynchronous master, however in my application it needs to be a synchronous slave to SAI1. I understand that there is no SAI2 FS signal output on a pin when in slave mode, but is the internal signal also disabled?

It's not working for me and I really hope there's an option or work around!

Many thanks,

Matt

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.