STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Stops in between without any error code.

Hello,I'm using STM32f723ZE controller & ADC configured as follow with external trigger(Timer), I verified timers works properly all the times and ADC 1 Stops after few minutes of data capture, but no error code set in Register. ADC1 & ADC2; (Externa...

TShet by Associate II
  • 826 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to use PC15 as GPIO input

Hello everyone,I'm working on a project using an stm32f030rc. I need to use PC15 as a GPIO input but it appears I'm unable to.I understand the couple PC14/PC15 is shared with the LFE oscillator, but of course I'm not using that function. Moreover, I ...

MMald.19 by Associate II
  • 2426 Views
  • 4 replies
  • 0 kudos

stm32f767zi max interrupt speed

I would have a question I am using stm32f767zi and trying to capture 2mhz signals with interrrupt600 700 khz is not much trouble, but 1mhzlerde starts to catch the deviation. Captures the rising and descending edgeI wonder how another method can be a...

MBOST by Associate
  • 837 Views
  • 1 replies
  • 0 kudos

Stm32f4disci power supply

I find a question. when I try to change the power for computer's USB interface to an extern 5V.it doesn't work.LD1 keep flashing.but when I use the computer's USB.it works well.what's wrong. I use it to produce a pwm.

Blly by Associate II
  • 3806 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.