STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! little fs for stm32h743ii

Dear all,I have dev a custom board  pcb based on stm32h743ii with 32MB of flash and 32MB  sdram FMC  for a 7 inch lcd HD. I am new on cubeide i coming from esp32 world and i have some programing dev question .Is it a good idear to implement :To parti...

KNaim.1 by Associate III
  • 1857 Views
  • 3 replies
  • 0 kudos

Exit from STOP2 mode in STM32u5g7

I am working with the STM32U5G7 microcontroller and have successfully implemented entry into STOP2 low-power mode. My system clock is 80Mhz(HSI, PLL), However, upon wake-up triggered via LPTIM . LPTIM is configured as counts internal clock events wit...

_Danny_ by Associate III
  • 1597 Views
  • 3 replies
  • 2 kudos

STM32H745 parallel transmission

Hi, I have Interface (type MASTER) 10-bit + CLK, FCLK=~9MHzCan I use DCMI to read 10-bit without VSYNC and HSYNC?Or some other method? The usual assembler software method "ldr r1, [port, #....]" is too slow and despite many attempts it has not been p...

EsKi by Associate II
  • 1976 Views
  • 5 replies
  • 0 kudos

Changing sample rate on streaming with H753 board

Hello, I am implementing audio streaming with H753 board. My goal is like below.     1. Input : USB connected PC, which can be selected one of 48kHz and 44.1kHz sample rate on connecting state. Others are fixed as 16 bit / 2 slot ( stereo )    2. Ou...

skson_0-1745198527483.png skson_1-1745199713895.png
skson by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos

GPIO Latency STM32F411 Blackpill

Hello All, I am doing this post after trying everything I can to solve my Issue. I have a STM32F411 Blackpill connected on an Apple II Bus Slot.The Apple II has a clock (Phi0) close to 1 Mhz. Phi0 is connected to Pin A2 where I have setup a Falling &...

Screen Shot 2025-05-08 at 20.56.06.png
vbesson by Senior
  • 5820 Views
  • 16 replies
  • 0 kudos

Resolved! STM32 F446RE Looses RTC Registers' Data When Power is Off

Hi all,I'm building a discharger using my STM F446RE, such that it's RTC registers are used to store data that'll be loaded to set parameters in my code every time the discharger is plugged into the power. Just to clarify - I'm NOT using the RTC as a...

nivg by Associate
  • 753 Views
  • 3 replies
  • 0 kudos

DFU mode STM32H7B3

Hello, we are facing some problem entering DFU mode from application code on our custom boards equipped with STM32H7B3 with bootloader release 0x92.  On contrary, everything works fine with same board equipped with STM32H7B3 bootloader release 0x91. ...

MMarco by Associate II
  • 5960 Views
  • 12 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.