STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! External QSPI with STM32H753

Hi, I am planning to use the external serial QSPI flash interface with STM32H753. Flash part number is MT25QL256ABA1EW7-0SIT or IS25LP064D-JKLE-TR. Operating voltage 3.3V at frequency of 80MHz DDR. Can you please let me know will there be any concern...

DJ_IND by Associate III
  • 1098 Views
  • 1 replies
  • 0 kudos

Resolved! System Clock stimluation error

I am using the startup file in Keil. However, when I run the simulation in the debugger, my system clock (SYSCLK) is not 72 MHz, even though I have confirmed that HSE_VALUE is set to 8 MHz.Can someone help me figure out why the SYSCLK is incorrect du...

sys clk.png

STM32H7 and openbootloader

Hi I'm implementing Openbootloader to my project, using an STM32H743, and is having a hard time finding the correct start addresses and size for "Option bytes registers". This is needed to in the "openbootloader_conf.h" file in the Openbootloader mid...

KFisc.2 by Associate II
  • 1526 Views
  • 1 replies
  • 1 kudos

Resolved! STM32U5 workshop GPDMA on U5A5

I followed the GPDMA tutorial here:https://www.youtube.com/watch?v=jKOhRfb3gvkand configured everything as shown.  The workshop was on a U575 but I would assume it's the same configuration for the U5A5?  I'm using the Nucleo-U5A5ZJ-Q.  I'm unable to ...

moylando by Associate III
  • 1253 Views
  • 2 replies
  • 0 kudos

Resolved! Floating-point arithmetic interrupts

Hello to everyone in the forum. I am using STM32H735.Is it possible to perform a floating point number operation and generate an interrupt when an exception occurs?I want to interrupt when the bit for exception generation in the FPSCR register is tur...

Hey0256 by Associate II
  • 1849 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.