STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H723 TIM2 in encoder mode not working

Hello, I have the following problem - I configured TIM2 of STM32H723 in Encoder Mode following all recommendations in the Reference Manual RM0468, chapter Encoder Interface Mode, p. 1694: • CC1S= 01 (TIMx_CCMR1 register, TI1FP1 mapped on TI1)• CC2S= ...

radekbg by Associate
  • 2006 Views
  • 3 replies
  • 1 kudos

Resolved! Clock frequency for STM32F303

Hi,I used to run my STM32F303RE at 72Mhz clock from a 8Mhz CMOS oscillator. . Timers8/1 operated at 72Mhz as well. That worked fine. I had to change the CMOS oscillator from 8 to 24Mhz.I tried two modifications, see attachment:a) I changed PLLMul fro...

DetlefS by Senior
  • 2834 Views
  • 5 replies
  • 4 kudos

STM32F411 Documentation-Reference Manual-Error

Hey, I just want to report an error in the Reference Manual for the STM32F411xC/E microcontroller.Reference Manual: https://www.st.com/resource/en/reference_manual/rm0383-stm32f411xce-advanced-armbased-32bit-mcus-stmicroelectronics.pdfPublished on: h...

wolkns by Associate
  • 951 Views
  • 1 replies
  • 1 kudos

Resolved! printf fail to print float type

Software tool: IAR Workbench 9.60#include <stdio.h>#include <math.h>#include <stdlib.h>#include <string.h>#include <intrinsics.h>int putchar( int ch ){    while(!(USART2->ISR&0X0080));   USART2->TDR  = (unsigned char)ch; return ch;} test code:printf(...

STM32L09 by Associate II
  • 1846 Views
  • 3 replies
  • 1 kudos

Resolved! FDCAN Not Transmitting or Receiving on STM32G0B1CCT6

I am working on FDCAN communication using an STM32G0B1CCT6 microcontroller. I am trying to perform a simple Tx/Rx loopback test (and later communication with external tools like Vehicle Spy), but I am facing the following problem: FDCAN is not trans...

AKG123 by Associate III
  • 7985 Views
  • 13 replies
  • 3 kudos

Resolved! Different stm32F103 behaving differently

I have purchased STM32F103c8t6 microcontrollers from three different vendors, but they are behaving differently.I am working on CAN, and on the microcontrollers from one vendor, it is working properly. But on the microcontrollers from other two vendo...

Gladson_2-1711604190715.png Gladson_0-1711603786582.png Gladson_1-1711604090049.png
Gladson by Associate III
  • 2740 Views
  • 2 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.