STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PWM jitter

Hello,  I am currently in the midst of developing a super simple system to create a varying load. It's basically to resistors in series with a transistor in parallel of the second resistor. The transistor is driven by a PWM signal to bypass the secon...

EliazLB by Associate III
  • 3976 Views
  • 5 replies
  • 2 kudos

STM32U575ZIT6 USB FS problem

Hello all, i got a firmware configuration problem, basically im using USB in FS modem and when i plug in the usb to  the pc what happens is that sometimes it can be recognized and i see a network disk called ''boot'' but most of times it cant be reco...

Resolved! STM32H7B3VIH6's LTDC does not generate pixel outputs

All control signals seem to be good: `DEN`, `VSYNC`, `HSYNC`, `CLK`. but pixel signals (R0 ~ R7, G0 ~ G7, B0 ~ B7) are always low. 1) DEN. 2) HSYNC. 3) VSYNC. 4) CLKalthough control signals correctly work, no pixel data lanes do not. Code that genera...

KakaoTalk_20250514_195533074.jpg KakaoTalk_20250514_195533074_01.jpg KakaoTalk_20250514_195533074_02.jpg KakaoTalk_20250514_195533074_03.jpg
jaehoon by Associate III
  • 1699 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H7RSxx TRM: MDIO CSR

Hi,The STM32H7RSxx  TRM  specifies, for ETH_MACMDIOAR, the following CSR values: Bits 11:8 CR[3:0]: CSR Clock RangeThe CSR Clock Range selection determines the frequency of the MDC clock according tothe CSR clock frequency (eth_hclk):0000: MDC clock ...

simo zz by Senior II
  • 1796 Views
  • 4 replies
  • 3 kudos

Resolved! Function to check flash page erased not working

I have the following function to verify that a full flash sector is erased but the code never seems to exit this function and I believe it gets stuck at the point where I dereference the address value. What could be the issue?static bool check_sector...

DMA with UART

Hello,I am trying to implement Modbus protocol in an efficient way. Untill now I have implemented everhting with UART interuot based Transmission and recption. Now I would like to implement with DMA to offload controller from much neavy lifting. For ...

Anesh by Associate III
  • 7715 Views
  • 16 replies
  • 2 kudos

Resolved! Initializing the HDP on STM32N6

I wanted to use the HDP (Hardware Debug Port) peripheral on the STM32N6 MCU (Nucleo N6 board), but CubeMX does not generate the MX_HDP_Init() function for it and does not initialize the peripheral either.Based on the reference manual, I tried configu...

hdp1-issue.png
pdemeter by Associate
  • 1173 Views
  • 1 replies
  • 1 kudos

error on address

I'm trying to use the LCD screen in STM32N6570DK, but it has an error like this`Break at address "0x18003a1a" with no debug information available, or outside of program code.`. But when I tried to view the vector table generated by disassembly, It wi...

creeper_0-1746500539292.png
creeper by Associate II
  • 1298 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.