2025-05-16 10:10 AM - last edited on 2025-05-16 11:05 AM by mƎALLEm
Hello,
I have the following problem - I configured TIM2 of STM32H723 in Encoder Mode following all recommendations in the Reference Manual RM0468, chapter Encoder Interface Mode, p. 1694:
• CC1S= 01 (TIMx_CCMR1 register, TI1FP1 mapped on TI1)
• CC2S= 01 (TIMx_CCMR2 register, TI2FP2 mapped on TI2)
• CC1P and CC1NP = ‘0’ (TIMx_CCER register, TI1FP1 noninverted, TI1FP1=TI1)
• CC2P and CC2NP = ‘0’ (TIMx_CCER register, TI2FP2 noninverted, TI2FP2=TI2)
• SMS= 011 (TIMx_SMCR register, both inputs are active on both rising and falling
edges)
• CEN= 1 (TIMx_CR1 register, Counter is enabled)
I also checked these settings in the TIM2 registers in debug mode with halting the micro and they were exactly as recommended. I checked the input quadrature signals - they are there. But still the TIM2 counter value stays 0 and does not change.
Any ideas what I might be missing?
Thanks a lot,
Radek
Solved! Go to Solution.
2025-05-18 1:17 PM
2025-05-18 2:59 AM
Read out and check/post the TIM and relevant GPIO registers content.
JW
2025-05-18 3:15 AM
The problem might be on my side - I am actually using the pair of channels CH3 and CH4 assuming they have the same functionality as the pair CH1 and CH2 which may be wrong?
2025-05-18 1:17 PM
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.