STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C011D6Y ADC input pin power consumption

Hi all,I'm working on a very low power custom board powered by a STM32C011D6Y micro controller. I must read an ADC input routed to F1 ball (PA3, PA4, PA5 or PA6) but I'm measuring some strange power consumption related to the input voltage on the pin...

Resolved! USART receiver timeout after a (LIN) BREAK?

Hi there,I am using the full featured USART in LIN mode. The start of a LIN packet is signaled by a BREAK condition. The next byte is the SYNC (0x55). After the BREAK is detected, I enable the receiver timeout so that if the SYNC (0x55) is not receiv...

STM32F411RE CAN Communication Project Issue

Hello,I am trying to build a part of the project.I want my three microcontrollers to communicate with each other via CANBus.What i am trying to achieve in this part is reading the digital sensor value from my hall effect sensor and sending this infor...

nwnd by Associate II
  • 4307 Views
  • 5 replies
  • 1 kudos

Resolved! How To Generate A Sine Wave With PWM And GPDMA (STM32H5)

Hi everyone, I'm trying to generate a sine wave using PWM output updated by GPDMA transfer on an STM32H5 device. I'm following this tutorial:STM32 Change PWM Duty Cycle With DMA For Sine Wave Generation However, when I try to implement it with STM32H...

Tzahi14_0-1746391670532.png Tzahi14_1-1746392320144.png Tzahi14_2-1746392622143.png
Tzahi14 by Associate
  • 2246 Views
  • 1 replies
  • 1 kudos

Resolved! STM32F402 part number, does it exist?

STM32World Rant #2 - MYSTERIOUS UNKNOWN MCUJust a short rant about the MYSTERIOUS STM32F402. This MCU does NOT exist in ST's catalog, and yet you can readily buy them in China. In this video I will go through the datasheet, find a comparable MCU whic...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.