STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407ZGT6 chip marking problem

我们这次购买的芯片上没有ARM标记,右上角的版本号改成了二维码的形式。 请咨询我们的供应商,不同的产地/包装厂/批次会有所不同。但是我们的质量部门不会库存它们。 标记的变化比较大。此标记更改是否有相应的文件? Translation: There is no ARM mark on the chip we purchased this time, and the version number in the upper right corner has been changed to a QR ...

微信图片_20240417104830.png 微信图片_20240417104847.png

Resolved! Trigger ADC with TIM2 TRGO not showing correct timing

Im using the following code that is part of a metal detector I'm building. Im trying to trigger the ADC based on TRGO of TIM2 (I need dma / adc readings every 10us after the of each TX pulse). I expect the TIM2_IRQHandler interrupt to enter 10us (ADC...

Resolved! VBUS not turning on on STM32H747I-DISCO

I am trying to configure the HS OTG port on the STM32H747I-DISCO dev board, but setting "Use external vbus" seems to be not enough. I can measure 0.8V on the CPEN line (measured from R11) but I don't see anything on the OUT line of the voltage switch...

chipchop by Associate II
  • 1123 Views
  • 1 replies
  • 0 kudos

The use of on-chip DACs in stm32g473cb

STM32G473CB has 3 DAC channel outputs.  a. Can these three DAC channels output a 100KHz triangle wave signal at the same time? b. In addition to the triangular wave, can the output signal output an irregular 100KHz waveform? thanks

licunxu by Associate II
  • 1196 Views
  • 3 replies
  • 0 kudos

STM32L552 LPTIM1 counter mode interupt

Hello,I'm new to stm32 microcontrollers. I'm trying to figure out how to configure LPTIM1 in counting mode, external clock in using cubeMX. Is there any examples on how to set it up?Is this even possible?Thanks in advance.

Hooks77 by Associate II
  • 932 Views
  • 1 replies
  • 1 kudos

Resolved! STM32G0B1KC USB device non recognized

Hi, I am using STM32G0B1KC ad usb device. I will show you all the conficuration for USB_DRD_FS and USB_DEVICE middleware.I am using the internal HSI48 for the USB clock.When I connect the device to my PC, the device is not recognized.Can anyone help ...

albvella_0-1747834958407.png albvella_1-1747835003419.png
albvella by Associate II
  • 1122 Views
  • 2 replies
  • 0 kudos

Impedance value of the pins

Hi, 1. In order to calculate the values of pull up & pull down resistor, in which section can we find the impedance information?2. Should we use external crystal for OSC_IN & OSC_OUT pins?3. If we are using USB2.0 FS feature what is the reference?Tha...

Meghna by Associate II
  • 1096 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.