2025-05-08 11:56 AM
Im using the following code that is part of a metal detector I'm building. Im trying to trigger the ADC based on TRGO of TIM2 (I need dma / adc readings every 10us after the of each TX pulse). I expect the TIM2_IRQHandler interrupt to enter 10us (ADC_DELAY_US) after the TX pulse ends (TIM1_CC_IRQHandler). I added a buffer (buffer variable) to keep track of the milliseconds of the events but when I print it on gdb (print buffer) and then subtract tx_end_micros to adc_start_micros, I dont have 10us, as expected:
This is a print of the gdb:
{{tx_end_micros = 2573435545, adc_start_micros = 2573437222, num_pulses = 2624525, num_pulses_tim2 = 2624526}, {tx_end_micros = 2573436545, adc_start_micros = 2573436542,
num_pulses = 2624526, num_pulses_tim2 = 2624527}}Below is the full code:
#include <stdio.h>
#include "stm32f4xx.h"
#include <math.h>
// Function Prototypes
void SystemClock_Config(void);
void GPIO_Init(void);
void TIM1_PWM_Init(void);
void TIM5_Init(void);
void LED_Init(void);
void TIM2_TRGO_Init(void);
void ADC1_Trigger_TIM2_Setup(void);
uint16_t adc1_read(void);
float compute_average(void);
void Delay_us(uint32_t);
void send_uart(char *msg);
uint32_t micros(void);
void toggle_led(void);
void enviar_dados_adc_serial(void);
void reset_adc(void);
// Settings
#define ADC_DELAY_US 10 // Delay after TX pulse before ADC sampling
#define NUM_SAMPLES 64 // Number of ADC samples to capture
// For alignment in memory
volatile uint16_t adc_buffer[NUM_SAMPLES] __attribute__((aligned(4)));
volatile uint32_t tx_num_pulses = 0;
volatile uint8_t adc_capture_complete = 0;
typedef struct {
uint32_t tx_end_micros;
uint32_t adc_start_micros;
uint32_t num_pulses;
uint32_t num_pulses_tim2;
} TimingData;
volatile TimingData buffer[2];
volatile uint8_t current_buffer = 0;
volatile TimingData timing; // Global instance, accessible in both ISRs
volatile uint32_t last_time;
volatile uint32_t curr_time = 0;
volatile uint32_t delta = 0;
void delay_ms(int milliseconds) {
volatile int i;
for (i = 0; i < milliseconds * 1000; i++) {
__NOP(); // No operation, just waste time
}
}
void reset_adc() {
// Reset DMA for next capture
ADC1->CR2 &= ~ADC_CR2_DMA; // Desliga DMA
ADC1->CR2 |= ADC_CR2_DMA; // Religa DMA
DMA2_Stream0->CR &= ~DMA_SxCR_EN;
while (DMA2_Stream0->CR & DMA_SxCR_EN);
// Clear DMA flags
DMA2->LIFCR |= DMA_LIFCR_CTCIF0 | DMA_LIFCR_CHTIF0 |
DMA_LIFCR_CTEIF0 | DMA_LIFCR_CDMEIF0 | DMA_LIFCR_CFEIF0;
// Reset DMA counter
DMA2_Stream0->NDTR = NUM_SAMPLES;
// Re-enable DMA
DMA2_Stream0->CR |= DMA_SxCR_EN;
}
void ADC1_Trigger_TIM2_Setup(void) {
RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN;
GPIOA->MODER |= (3 << (1 * 2)); // PA1 analog mode
ADC1->CR2 = 0; // rests all (not using continuous capture)
ADC1->CR2 |= ADC_CR2_ADON;
Delay_us(1); // Small delay for ADC stabilization
ADC1->SMPR2 = 0; // 3 cycles sampling time (channels 0-9)
ADC1->SQR3 = 1; // Channel 1 (PA1)
// Configure for TIM2_TRGO triggering
ADC1->CR2 &= ~(0xF << ADC_CR2_EXTSEL_Pos); // Clear EXTSEL
ADC1->CR2 |= (6 << ADC_CR2_EXTSEL_Pos); // TIM2_TRGO
ADC1->CR2 |= (1 << ADC_CR2_EXTEN_Pos); // Rising edge
// Configure DMA
ADC1->CR2 |= ADC_CR2_DMA; // Enable DMA
ADC1->CR2 &= ~ADC_CR2_CONT; // Desativa modo contínuo
}
void TIM2_TRGO_Init(void) {
RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
TIM2->PSC = 84 - 1; // 1 µs per tick
TIM2->ARR = ADC_DELAY_US - 1; // Count to delay value
TIM2->CNT = 0;
// Configure TIM2 to generate TRGO on Update event
TIM2->CR2 &= ~TIM_CR2_MMS;
TIM2->CR2 |= TIM_CR2_MMS_1; // MMS = 010 = Update Event
// Configure TIM2 as slave of TIM1 in Trigger mode (starts when receiving trigger)
TIM2->SMCR &= ~(TIM_SMCR_SMS | TIM_SMCR_TS); // Clear all
TIM2->SMCR |= (0x6 << TIM_SMCR_SMS_Pos); // SMS=110 (Trigger Mode)
TIM2->SMCR |= (0x0 << TIM_SMCR_TS_Pos); // TS=000 (ITR0 = TIM1)
TIM2->SMCR |= (0x6 << TIM_SMCR_SMS_Pos); // SMS=110 (Trigger Mode)
// Enable one-pulse mode so TIM2 stops after one cycle (form dma in non circular mode)
// TIM2->CR1 |= TIM_CR1_OPM;
// Enable update interrupt for TIM2
TIM2->DIER |= TIM_DIER_UIE;
NVIC_EnableIRQ(TIM2_IRQn);
}
void DMA2_Stream0_ADC_Config(void) {
RCC->AHB1ENR |= RCC_AHB1ENR_DMA2EN; // Enable DMA2 clock
// Make sure stream is disabled
DMA2_Stream0->CR &= ~DMA_SxCR_EN;
while (DMA2_Stream0->CR & DMA_SxCR_EN); // Wait for deactivation
// Clear interrupt flags
DMA2->LIFCR |= DMA_LIFCR_CTCIF0 | DMA_LIFCR_CHTIF0 |
DMA_LIFCR_CTEIF0 | DMA_LIFCR_CDMEIF0 | DMA_LIFCR_CFEIF0;
// Configure peripheral address (ADC1_DR)
DMA2_Stream0->PAR = (uint32_t)&ADC1->DR;
// Buffer address in memory
DMA2_Stream0->M0AR = (uint32_t)&adc_buffer;
// Number of transfers
DMA2_Stream0->NDTR = NUM_SAMPLES;
// Configure for channel 0 (ADC1)
DMA2_Stream0->CR =
(0 << DMA_SxCR_CHSEL_Pos) | // Channel 0
(1 << DMA_SxCR_MSIZE_Pos) | // Memory 16 bits
(1 << DMA_SxCR_PSIZE_Pos) | // Peripheral 16 bits
(1 << DMA_SxCR_MINC_Pos) | // Increment memory
(0 << DMA_SxCR_PINC_Pos) | // Don't increment peripheral
(0 << DMA_SxCR_CIRC_Pos) | // Normal mode (not circular) circular 1
(0 << DMA_SxCR_DIR_Pos) | // Peripheral -> Memory
(1 << DMA_SxCR_TCIE_Pos); // Transfer complete interrupt
// Enable DMA interrupt
NVIC_EnableIRQ(DMA2_Stream0_IRQn);
}
void toggle_led() {
GPIOD->ODR |= (1 << 12); // Turn LED on
Delay_us(10);
GPIOD->ODR &= ~(1 << 12); // Turn LED off
}
void uart_init(void) {
// Enable clocks for GPIOA and USART1
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN;
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
// Configure PA9 and PA10 for alternate function (AF7)
// TX = PA9, RX = PA10
GPIOA->MODER &= ~((3 << (9 * 2)) | (3 << (10 * 2))); // clear bits
GPIOA->MODER |= (2 << (9 * 2)) | (2 << (10 * 2)); // alternate function mode
GPIOA->AFR[1] &= ~((0xF << ((9 - 8) * 4)) | (0xF << ((10 - 8) * 4)));
GPIOA->AFR[1] |= (7 << ((9 - 8) * 4)) | (7 << ((10 - 8) * 4)); // AF7 (USART1)
// Configure USART1: 115200 baud, 8N1
USART1->BRR = 0x2D9; // For 115200 baud with PCLK2 = 84 MHz
USART1->CR1 = USART_CR1_TE | USART_CR1_UE; // Enable transmitter and USART
}
void send_uart(char *msg) {
while (*msg) {
while (!(USART1->SR & USART_SR_TXE)); // wait for empty buffer
USART1->DR = *msg++;
}
}
int main(void) {
// Configure system clock
SystemClock_Config();
// Initialize UART for debug via serial
uart_init();
// Initialize GPIO (PE13 as TIM1_CH3 Alternate Function)
GPIO_Init();
LED_Init();
TIM5_Init();
// Initialize TIM1 for PWM on PE13
TIM1_PWM_Init();
// Initialize TIM2 for ADC triggering
TIM2_TRGO_Init();
// Configure ADC and DMA
DMA2_Stream0_ADC_Config();
ADC1_Trigger_TIM2_Setup();
while (1) {
if (adc_capture_complete) {
// Reset flag
adc_capture_complete = 0;
/* // Reset DMA for next capture
ADC1->CR2 &= ~ADC_CR2_DMA; // Desliga DMA
ADC1->CR2 |= ADC_CR2_DMA; // Religa DMA
DMA2_Stream0->CR &= ~DMA_SxCR_EN;
while (DMA2_Stream0->CR & DMA_SxCR_EN);
// Clear DMA flags
DMA2->LIFCR |= DMA_LIFCR_CTCIF0 | DMA_LIFCR_CHTIF0 |
DMA_LIFCR_CTEIF0 | DMA_LIFCR_CDMEIF0 | DMA_LIFCR_CFEIF0;
// Reset DMA counter
DMA2_Stream0->NDTR = NUM_SAMPLES;
// Re-enable DMA
DMA2_Stream0->CR |= DMA_SxCR_EN; */
}
}
}
void SystemClock_Config(void) {
// 1. Enable HSE (High-Speed External Clock, typically 8 MHz)
RCC->CR |= RCC_CR_HSEON;
while (!(RCC->CR & RCC_CR_HSERDY)); // Wait for HSE to stabilize
// 2. Configure PLL to multiply frequency
RCC->PLLCFGR = (8 << RCC_PLLCFGR_PLLM_Pos) | // HSE 8MHz /8 = 1MHz
(336 << RCC_PLLCFGR_PLLN_Pos) | // 1MHz × 336 = 336MHz
(0 << RCC_PLLCFGR_PLLP_Pos) | // 00 = divide by 2 → 168MHz
(7 << RCC_PLLCFGR_PLLQ_Pos) | // USB clock = 336/7 = 48MHz
RCC_PLLCFGR_PLLSRC_HSE; // Use HSE as source
// 3. Activate PLL
RCC->CR |= RCC_CR_PLLON;
while (!(RCC->CR & RCC_CR_PLLRDY)); // Wait for PLL to stabilize
// 4. Configure bus frequencies to avoid overclock
RCC->CFGR |= RCC_CFGR_HPRE_DIV1; // AHB Prescaler = 1 (168 MHz)
RCC->CFGR |= RCC_CFGR_PPRE1_DIV4; // APB1 Prescaler = 4 (42 MHz)
RCC->CFGR |= RCC_CFGR_PPRE2_DIV2; // APB2 Prescaler = 2 (84 MHz)
FLASH->ACR |= FLASH_ACR_LATENCY_5WS | FLASH_ACR_PRFTEN | FLASH_ACR_ICEN | FLASH_ACR_DCEN;
// 6. Switch System Clock to PLL
RCC->CFGR |= RCC_CFGR_SW_PLL;
while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL); // Wait for switch
// Configure ADC clock
ADC->CCR &= ~ADC_CCR_ADCPRE; // Clear ADCPRE bits
ADC->CCR |= (3 << ADC_CCR_ADCPRE_Pos); // 11b → divide APB2 por 8 → ADCCLK = 84 / 8 = 10.5 MHz :white_heavy_check_mark:
SystemCoreClockUpdate();
}
void GPIO_Init(void) {
// Enable clocks for GPIOs A and E
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; // Enable GPIOA clock (for PA8)
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOEEN; // Enable GPIOE clock
// Configure PE13 as alternate function (TIM1_CH3)
GPIOE->MODER &= ~(3 << (13 * 2));
GPIOE->MODER |= (2 << (13 * 2)); // Alternate function mode
GPIOE->OSPEEDR |= (3 << (13 * 2)); // High speed for PE13
GPIOE->AFR[1] &= ~(0xF << ((13 - 8) * 4)); // Clear AFR[1] bits for PE13
GPIOE->AFR[1] |= (1 << ((13 - 8) * 4)); // Set AF1 for PE13 (TIM1_CH3)
// Configure PA8 as alternate function (TIM1_CH1)
GPIOA->MODER &= ~(3 << (8 * 2));
GPIOA->MODER |= (2 << (8 * 2)); // Alternate function mode
GPIOA->OSPEEDR |= (3 << (8 * 2)); // High speed
GPIOA->AFR[1] &= ~(0xF << ((8 - 8) * 4)); // Clear AF bits
GPIOA->AFR[1] |= (1 << ((8 - 8) * 4)); // AF1 (TIM1_CH1)
// Configure PA1 as analog input for ADC
GPIOA->MODER |= GPIO_MODER_MODER1; // Analog mode (0b11)
// Debug pin (set PE1 as debug pin)
GPIOE->MODER |= (1 << (1 * 2)); // PE1 as output
GPIOE->ODR &= ~(1 << 1); // Start low
}
// Timer used only for debug timing
void TIM5_Init(void) {
// Enable clock for TIM5
RCC->APB1ENR |= RCC_APB1ENR_TIM5EN;
// APB1 is 42MHz, but timer clock is 2x that (84MHz)
// For 1 µs resolution: 84MHz / 84 = 1MHz
TIM5->PSC = 84 - 1;
// Max auto-reload (32 bits)
TIM5->ARR = 0xFFFFFFFF;
// Start counting
TIM5->CR1 |= TIM_CR1_CEN;
// Reset TIM5 counter
TIM5->CNT = 0;
}
uint32_t micros(void) {
return TIM5->CNT;
}
void TIM1_PWM_Init(void) {
// Enable TIM1 clock on APB2 bus
RCC->APB2ENR |= RCC_APB2ENR_TIM1EN;
// Set timer frequency (reduce clock to 1 MHz, so 1 tick = 1 µs)
TIM1->PSC = 168-1; // Prescaler (divides timer clock)
// Set PWM period (1ms = 1000 µs)
TIM1->ARR = 1000 - 1; // Define maximum count (PWM period)
// Set duty cycle (100 µs)
TIM1->CCR3 = 100; // TX pulse width
TIM1->CCR1 = 500; // 500µs pulse width (for PA8)
// Configure TIM1 Channel 3 for PWM1 mode
TIM1->CCMR2 &= ~TIM_CCMR2_OC3M; // Clear output mode bits for Channel 3
TIM1->CCMR2 |= (6 << TIM_CCMR2_OC3M_Pos); // Set Channel 3 to PWM1 mode
TIM1->CCMR2 |= TIM_CCMR2_OC3PE; // Enable Preload for CCR3
// Configure polarity (active high)
TIM1->CCER &= ~TIM_CCER_CC3P;
TIM1->CCER |= TIM_CCER_CC3E; // Enable PWM output on Channel 3
// Configure Channel 1 (for PA8 charge pump pulse) as PWM Mode 1
TIM1->CCMR1 &= ~TIM_CCMR1_OC1M;
TIM1->CCMR1 |= (6 << TIM_CCMR1_OC1M_Pos); // PWM Mode 1
TIM1->CCMR1 |= TIM_CCMR1_OC1PE; // Enable preload
// Configure polarity (active high) and enable output
TIM1->CCER &= ~TIM_CCER_CC1P; // Active high
TIM1->CCER |= TIM_CCER_CC1E; // Enable output
// Configure TIM1 to generate TRGO on OC3REF signal (when TX pulse ends)
TIM1->CR2 &= ~TIM_CR2_MMS;
//TIM1->CR2 |= TIM_CR2_MMS_1 | TIM_CR2_MMS_0; // MMS = 011 = OC3REF as trigger
// TIM1->CR2 |= (TIM_CR2_MMS_1 | TIM_CR2_MMS_0);
TIM1->CR2 |= (0x3 << TIM_CR2_MMS_Pos); // MMS=011 (OC3REF = PWM end)
// Enable interrupt at compare match (when CCR3 is reached)
TIM1->DIER |= TIM_DIER_CC3IE;
// Enable both compare and update interrupts
TIM1->DIER |= TIM_DIER_CC3IE | TIM_DIER_UIE;
NVIC_EnableIRQ(TIM1_UP_TIM10_IRQn); // Enable update interrupt
NVIC_EnableIRQ(TIM1_CC_IRQn); // Enable compare interrupt
// Start TIM1 counter, generating PWM
TIM1->CR1 |= TIM_CR1_CEN;
// Enable PWM output on physical pins (only for advanced timers like TIM1 and TIM8)
TIM1->BDTR |= TIM_BDTR_MOE;
}
void LED_Init(void) {
RCC->AHB1ENR |= RCC_AHB1ENR_GPIODEN;
GPIOD->MODER |= (1 << (12 * 2));
GPIOD->ODR &= ~(1 << 12); // Ensure LED starts off
}
uint16_t adc1_read(void) {
ADC1->CR2 |= ADC_CR2_SWSTART; // Start conversion
while (!(ADC1->SR & ADC_SR_EOC)); // Wait until conversion complete
return ADC1->DR; // Read result
}
/* === Interrupt Handlers === */
// TIM1 update interrupt handler (debug: used only for debug of TX pulse start with LED)
void TIM1_UP_TIM10_IRQHandler(void) {
if (TIM1->SR & TIM_SR_UIF) {
TIM1->SR &= ~TIM_SR_UIF;
// TX pulse start logic here if needed
}
}
// TIM1 compare interrupt handler (at end of TX pulse)
void TIM1_CC_IRQHandler(void) {
if (TIM1->SR & TIM_SR_CC3IF) {
TIM1->SR &= ~TIM_SR_CC3IF;
tx_num_pulses++;
buffer[current_buffer].tx_end_micros = micros();
buffer[current_buffer].num_pulses = tx_num_pulses;
uint8_t buf = current_buffer ^ 1;
current_buffer = buf;
}
}
void TIM2_IRQHandler(void) {
// Check if update interrupt occurred
if (TIM2->SR & TIM_SR_UIF) {
TIM2->SR &= ~TIM_SR_UIF; // Clear interrupt flag
buffer[current_buffer].adc_start_micros = micros();
buffer[current_buffer].num_pulses_tim2 = tx_num_pulses;
}
}
void DMA2_Stream0_IRQHandler(void) {
if (DMA2->LISR & DMA_LISR_TCIF0) {
// Clear the transfer complete flag
DMA2->LIFCR |= DMA_LIFCR_CTCIF0;
adc_capture_complete = 1;
}
}
// --- Utilities ---
void Delay_us(uint32_t us) {
volatile uint32_t count = us * (SystemCoreClock / 1000000) / 5;
while (count--);
}
Solved! Go to Solution.
2025-05-12 3:36 AM
Hello @cristianosar,
With TIM2->PSC = 84 - 1; and TIM2->ARR = ADC_DELAY_US - 1, this configuration should give you a 10 µs delay, if your timer clock is 84 MHz
Also, If you want TIM2 to stop after one cycle, this line (TIM2->CR1 |= TIM_CR1_OPM) should be uncommented.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-12 3:36 AM
Hello @cristianosar,
With TIM2->PSC = 84 - 1; and TIM2->ARR = ADC_DELAY_US - 1, this configuration should give you a 10 µs delay, if your timer clock is 84 MHz
Also, If you want TIM2 to stop after one cycle, this line (TIM2->CR1 |= TIM_CR1_OPM) should be uncommented.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-22 12:34 PM
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.