STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DFSDM decimated frequency

Hi I have a simple question about DFSDM configuration. I want to apply sinc5 with 32 samples length and therefore get 32 times decimation. Btw, I use internal ADC1/ADC2 in dual mode. STM32H725.Thus, for a given ADC frequency F I expect to get decimat...

LeonidP by Associate III
  • 1170 Views
  • 1 replies
  • 0 kudos

STM32G051 - Current Control, Cycle by Cycle

Hello,I am new with STM32. We would like to do a current control exactly like on this document :https://www.st.com/resource/en/product_training/STM32G0-Analog-Comparators-COMP.pdfpage 13But we would like to use COMP1 for ZCD and COMP2 for overcurrent...

Marc38_0-1744274148620.png Marc38_3-1744276720125.png
Marc38 by Associate II
  • 2700 Views
  • 6 replies
  • 3 kudos

Resolved! Differences between F411RE and F767ZI SPI interfaces?

Hi,I am accessing a DRV8873s motor driver (SPI version) on two different NUCLEO boards. My usage is limited to reading data from 2 registries.I got it to work on a NUCLEO-STM32F411RE using SPI2, with the following settings:Motorola format, 8 bits, MS...

RH38 by Associate II
  • 2325 Views
  • 6 replies
  • 2 kudos

Resolved! Transaction error trying to use DMA to write to GPIO

I've been trying to set up a timer and DMA to run a synchronous parallel bus onto a GPIO. The timer works great but the DMA keeps failing with a transaction error interrupt and disables the stream. This is on an STM32F413 chip and using TIM2_CH1 as a...

Elin by Associate II
  • 2002 Views
  • 5 replies
  • 0 kudos

STM32H7S7 XSPI Thermal Issues

Hi there, We are having some issues with our STM32H7 when the MCU is heated above approximately 55C. This leads to a fault of some form within the STM32 which prevents it from reading an external flash which the code is being run from. This memory is...

RobertT by Associate II
  • 2282 Views
  • 5 replies
  • 1 kudos

STM32F101C8 Boot Loader reload?

Hello, New here. I am working with a piece of consumer electronics equipment that uses a STM32F101C8 processor. the customer was doing an update to this unit and in the middle of the update, pulled the USB plug out of his computer bricking the unit. ...

Resolved! Usage of ULPI & CANFD interfaces

I want to use the ULPI interface & both the CAN interface for my project But I see  For USB:   Pin No: 194     pin name: PB5     Module function :  USB_OTG_HS_ULPI_D7,   ONLY ONE PIN no other pins are there   For CAN   Pin No: 194,195    pin name: PB...

Meghna by Associate II
  • 2854 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.