STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with option bytes set from program level- G0B1

Hi! I have problem with setting option bytes from program. Setting OBs from Cube Programmer working good. MCU im using is STM32G0B1.  I found and implement this function:   HAL_StatusTypeDef optionByteSetBootFromPin(void) { FLASH_OBProgramInitTypeD...

BPrac.1 by Associate III
  • 4074 Views
  • 4 replies
  • 1 kudos

Resolved! question about stm32h750bdk ExtMem_boot

 Inside the QSPI_EnableMemoryMappedMode function, the dummy cycles are MT25TL01G_DUMMY_CYCLES_READ_QUAD_DTR - 1.MT25TL01G_DUMMY_CYCLES_READ_QUAD_DTR is defined as 6U.The datasheet for MT25TL01G states that the DTR QUAD INPUT/OUTPUT FAST READ value is...

taeun by Associate II
  • 2717 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F105RC USB Device not detected

Hello.  I have a custom board with F105RCT7. The summary of my problem is the USB interface is not working at all. The computer does not detect anyting. The board is configured as a VCP device. I have a Nucleo-H743ZI-2 board and done some tests with....

hckar_0-1747988544280.png Cattura.PNG
hckar by Associate II
  • 2874 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.