2025-05-26 8:32 PM
I want to configure IDMA in the sdmmc interface of H750, but I can't find a sample, is there a tutorial?
i use stm32cubemx as the toolchain
2025-05-27 6:57 AM
Hi @uestc
Please refer to the Reference Manual RM0443, specifically section "55.5.6 SDMMC AHB Master Interface" which can help you to configure IDMA in the SDMMC interface.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.