STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407ZET6 Could not verify ST Device

Hi All, I have a setup where I bought a STM32F407ZET6 dev board from AliExpress and have been using for almost 6 years using STM32Cube IDE. It was only until i updated my IDE from 1.6 to 1.14 when it started saying that "Could not verify ST Device! P...

Neolithic_0-1702623539327.png
Neolithic by Associate III
  • 12761 Views
  • 19 replies
  • 8 kudos

timer 3 channel 2 pwm influence channel 4

Using stm32h743 device. when configuring timer 3 as pwm on channel 1 with phase on channel 2, we see that channel 4 will be influenced by channel 2even though channel 4 was not defined.if i configured channel 3 and 4 for pwm and phase i will have the...

dorong by Associate II
  • 1505 Views
  • 4 replies
  • 0 kudos

Resolved! RWW for Single Bank Flash on STM32

I understand you can't erase the same bank you are running code in. Or something like that. But I am confused on the STMG0 because this one only has a single bank. So how do I use Flash to emulate EEPROM if I am using flash to run my code. Everything...

Carl_G by Senior III
  • 3134 Views
  • 8 replies
  • 1 kudos

Resolved! STM32H750 FDCAN Not transmiting

Dear Sirs,I am implementing an interface between an STM32H750 and a CanBus device of an electric bike. I have the FDCAN peripheral configured to 250kbit/s (FDCAN clock is 48MHz)I have to interface with devices that use Extended Frames, but the speed ...

VCasa3_0-1748185676203.png VCasa3_1-1748185692372.png
VCasa.3 by Associate II
  • 1420 Views
  • 2 replies
  • 2 kudos

Unexpected PB3 behavior with connected st-link

Moved from Feedback forum. The Feedback forum is for feedback about the forum itself - not product questions. Hello! During project debugging i encountered with follow situation. I have a led connected to PB3 pin (configured as output push-pull with...

STM32G030 - FLASH - Fail to use FLASH_Program_Fast

Hi!I am using STMCube IDE and a STM32G030F6I am trying to implement a code that writes variables to the flash. And I was able to make it work, with some limitations...THIS CODE WORKSunion  {  uint8_t regs[6];  uint64_t data;  } mem;    uint64_t *my...

arthhh by Associate II
  • 3051 Views
  • 4 replies
  • 1 kudos

STM32F429 Boot Slow

Hello  I wrote a BootLoader program and an app program  in flash,BootLoader program will Jump to app. current state is,BootLoader boot takes a longtime,and jump also takes a longtime, the length of  time  positively correlated with the size of global...

QingFeng by Associate II
  • 741 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H730 HyperRam issue

I have a custom board with a STM32H730 and an IS66WVH32M8 HyperRam.The ram is connected on octospi1 outputs.I can read and write in indirect mode to the internal registers of the ram.But in memory mapped mode i read only wrong values.To test the ram ...

Roba by Associate
  • 1806 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.