STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32h743ii 2 i2c independant bus

 Dear all; I have a *** question but it dont work can we have quantity 2 different i2c bus 1 is reconized but not the second bus  /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_LTDC_Init(); MX_QUADSPI_Init(); MX_FMC_Init(); ...

KNaim.1 by Associate III
  • 2246 Views
  • 6 replies
  • 3 kudos

Questions on FMC throughput with DMA

I'm working on a project which uses DMA to pull data from an external chip controlled by the FMC into a buffer in AXI SRAM, and am seeing a much lower throughput than expected. It looks like the FMC is idle for long periods of time, and I'm looking f...

8-bit-dma-capture.png 32-bit-dma-capture.png 64-bit-core-capture.png
BenDDMC by Associate
  • 965 Views
  • 0 replies
  • 0 kudos

UART RS485 how to manage half-duplex

Hello,I implement RS-485 on STM32G491. I receive with ReceiveToIdle_DMA and I also transmit with DMA. I need to know if currently something is being received because that means I cannot send data now because RS485 is half-duplex. As far as I know I c...

Ramzes11 by Associate
  • 3122 Views
  • 4 replies
  • 2 kudos

Resolved! STM32L431KCUX UART cannot receive more than 49 bytes

Recently I have encountered a strange issue I cannot really explain...I have a firmware that manages serial UART communication with a callback that has a state machine with 3 states.In the first state, UART is set to perpetually expect 1 byte of data...

MO94 by Associate III
  • 4565 Views
  • 15 replies
  • 8 kudos

Resolved! LPTIMER fail to wakeup in STOP2 mode for longer timeout

Hello,Trying to achieve wakeup system at every 60 sec or more using LPTIMER1 in STOP2 mode.Observation:1. STOP2 = enable and LPTIMER = 60 sec --> Wakeup not work2. STOP2 = disable and LPTIMER = 60 sec --> Wakeup work3. STOP2 = enable and LPTIMER = 2 ...

Resolved! Is a bootloader necessary?

can anybody answer please, if i costmised board based on  bg431besc1 board  it needed to upload boot loader file in stm32g431 controller to run in stm32ide code ?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.