2024-05-01 8:00 AM
Hi all,
Is there a Modbus tcp/ip Server (Slave) and client (Master) examples for STM32 Nucleo F429ZI board or any other similar boards?
Thanks,
Solved! Go to Solution.
2024-05-29 4:01 AM
Hello,
Currently, we do not have any examples implementing MODBUS protocol over TCP/IP. After doing a quick search, I found the links below that I think could help you. You could try and salvage what you can and adapt it to the board you are using.
I also suggest you take a look at LWIP TCP client/server examples for other boards from our STM32Cube FW package (for example LwIP_TCP_Echo_Client, LwIP_TCP_Echo_Server) as you could use them to extract a template code for client/server communication.
Best regards,
2024-05-29 4:01 AM
Hello,
Currently, we do not have any examples implementing MODBUS protocol over TCP/IP. After doing a quick search, I found the links below that I think could help you. You could try and salvage what you can and adapt it to the board you are using.
I also suggest you take a look at LWIP TCP client/server examples for other boards from our STM32Cube FW package (for example LwIP_TCP_Echo_Client, LwIP_TCP_Echo_Server) as you could use them to extract a template code for client/server communication.
Best regards,
2024-07-21 2:22 AM
Hi data_cracker
I've just come across your question - I'm trying exactly the same thing, did you make any progress on your project with Modbus TCP on Nucleo?
Thanks
2025-05-29 7:39 AM
I am also going to try this out. I need to establish a ModbusTCP connection between the STM32H7 NUCLEO board with an RJ-45 ethernet port. Has anyone had any success getting it to work with the HAL & FreeRTOS option above? I was looking for a native option using just code.
I was watching this video: Mastering Modbus TCP: STM32 as a Slave - Read & Write Registers - YouTube
where he is using the Mongoose library.
I'm just starting here. First time using an STM32 and hoping to have some success.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.