Resolved! What is the ADC sampling rate of STM32F103?
I want to know the ADC performance of STM32F103.I am not sure which datasheet to check.I know it is single ended in SAR ADC....I'd really appreciate it if you let me know.
Ask questions, find answers, and share insights on STM32 products and their technical features.
I want to know the ADC performance of STM32F103.I am not sure which datasheet to check.I know it is single ended in SAR ADC....I'd really appreciate it if you let me know.
Moin, is it possible to run the stm32L5 Series mcus (or other stm32s) not in SDMMC host mode, but be used like a normal SDcard for storage?I looked over the documentation and only found host mode descriptions. I feel like I missed some details, so gr...
Hello all =)I am pretty much a beginner with STM32 microcontrollers and facing some, at least for me, elusive problems during debugging of the controller.I am working with the SENSORTILE, so the STM32L476JG controller, which is soldered onto the crad...
In my project there is requirement to initialize the IWDG for two times one with time period 5 second in run-mode and re-configuring it for 32 second before controller enters into sleep mode. as shown in below code. hiwdg.Instance = IWDG; hiwdg.Ini...
In STM System WorkBench : Can we use 2 different linker scripts , one for Debug Settings and one for the Release setting . Currently there is no option to exclude one linker script when switching between Release Configuration to Debug configuration
Hello, I've been trying to flash the STM32L0538 DISCO with a blink sketch after years of not touching it. Every thing seem to work fine led blinking and stuff the DISCO board look relatively new after 2+ years but when I come to upgrade the st link t...
I am trying to flash options bytes on a STM32H7 via the code below. Both the code snippets return HAL_ERROR from the HAL_FLASH_OB_Launch(). What am I doing wrong?I am referring to the following STM32Cube example code: https://github.com/STMicroelectr...
We are currently using an F4 (STM32F407IGH6) and an F3 (STM32F303VC) in our product. We want to pull the temperature sensors to get an idea of chip temp. Looking at the datasheets, the F3 data sheet explicitly states that factory calibraiton is done...
Hi,I want to use an ADC with DMA in a STM32F103. I configured it in Cube as you can see in the following picures.When I start the conversion with HAL_ADC_Start_DMA(&hadc1,(uint32_t*)AdcData,5);HAL_ADC_ConvCpltCallback() is called and I see that the A...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.