STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

any stm32 MCU with 5Vadc?

Hello,I am working on a project and it would be very helpful if I could find a MCU with integrated 5V ADC. I know you can add a voltage divider for the 3.3V ADC but it won't work in my case for this project. Can anyone recommend me something? Thank y...

retro by Associate III
  • 2210 Views
  • 4 replies
  • 0 kudos

SWD printf debuggin issues..

Hello,I'm just a beginner that tryes to migrate from the arduino world to ST and before I start the dev jorney I'd like to hand on to a debbuging method that requiers as little hardware and sofware setup as possible while still having the logging and...

MLemo.1 by Associate III
  • 2862 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G071 DMA Will Not Transfer Data to UART1 TDR

I'm trying to operate the USART in DMA tx mode on the STM32G0. I've configured the DMA mux to route the USART1TX dma request to channel 2. I have configured channel 2 to enable TC and TE interrupts, enabled MINC, and set PSIZE & MSIZE as byte. The nu...

CKafk.1 by Associate II
  • 3286 Views
  • 6 replies
  • 0 kudos

RTC_EnterInitMode(hrtc) returns HAL_TIMEOUT. LSEState is ON and HAL_PWR_EnableBkUpAccess() is also called. How to solve this issue?

HAL_StatusTypeDef HAL_RTC_DeInit(RTC_HandleTypeDef *hrtc) function returns HAL_ERROR because RTC_EnterInitMode(hrtc) returns HAL_TIMEOUT. When checked in community, I can see solutions as to call HAL_PWR_EnableBkUpAccess(); before setting RTC functio...

RVarg.1 by Associate
  • 2072 Views
  • 3 replies
  • 0 kudos

Resolved! Fault when casting from char* to uint64_t*

In my code, I write many casting from char* to uint64_t*. Someone success, and someone get failure. I thought I used the unallocated memory, but I rewrote by casting to uint32_t, and then no error happened. Is this normal?My code:--------------------...

Ellaine by Associate II
  • 3151 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F469i Source Code for Demo Firmware

Hello all,I recently purchased the STM32F469i Discovery Board, and have loaded the compiled demo binary from the ST website onto the board. It loads properly, but now I want to see how the software works. Is there any source code for the demo firmwar...

TLian.11 by Associate II
  • 1475 Views
  • 2 replies
  • 0 kudos

STM32F767 QUAD SPI with DMA2

I'm using STM32F767 and external flash is interfaced on QUADSPI, I've referred STM32746G-Discovery code for QSPI without DMA and its working fine. I want to implement QSPI using DMA, STM32F767 supports QSPI over DMA on channel 3 and stream 7 so did c...

AShel.1 by Associate III
  • 1379 Views
  • 2 replies
  • 0 kudos

Can't wake from stop mode with low power timer event

Hello everyone,I'm having problems with a STM32L010K8 in stop mode.I'm trying to use the low power timer clocked by the LSI and having it to wake up the device from stop mode once the timer reaches ARR value.I configured the EXTI event line 29 and de...

Kraal by Lead
  • 4136 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.