2020-07-10 5:09 AM
Moin,
is it possible to run the stm32L5 Series mcus (or other stm32s) not in SDMMC host mode, but be used like a normal SDcard for storage?
I looked over the documentation and only found host mode descriptions. I feel like I missed some details, so greatly appreciate pointers.
Cheers
2020-07-10 5:48 AM
No, this generally requires IP to act as a state machine, or buffering/protocol engine.
You could be a SPI slave, and respond/interface that way, but the performance would be incredibly lackluster.
2020-07-10 6:02 AM
Thanks!
I had the naive assumption it "should" be possible and hence kept looking.
Cheers
2020-07-10 6:11 AM
Generally specialized devices used as NAND controllers, or interfacing WiFi controller IC.
The mechanics could probably be plumbed via an FPGA/CPLD, but STM32 parts don't really provide for an external DMA interface (ie inbound/outbound interface to internal memories), but only an external memory interface into which you could map your own peripherals or memory buffers.
SPI would be a means to act like a faux SD Card, but generally the effort would be high and the rewards low, and why there's probably no pre-package solution
2020-07-10 6:20 AM
yes. totally agree. Once I realized sdmmc was running at 25MHz I started to have doubts. Without the corresponding (lacking) IP it will just be a mess. A small fpga will most likely be used in this project then.
I will try it with SPI for fun, but I doubt to get meaningful results in terms of speed and will push it to weekend project with an stm32.
Thanks again!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.