STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Host With Multiple Vendor Specific Devices

Posted on August 28, 2014 at 22:23I'm new to USB programming, and am having some trouble getting my head around the concepts involved.  Hopefully someone can have a look at what I think I need to do to meet my goals and tell me where I'm right and w...

jwormsley by Associate III
  • 15355 Views
  • 24 replies
  • 2 kudos

Resolved! STM32F410 Bat voltage measurement consumption

Hi everyone,I was just wondering if measuring VBat in continuous will drain the battery faster ? And how fast ?Unfortunately, I don't have tools that should be able to measure such a low current.I use the STM32F410CB in my project. I use the adc1 (th...

RSchl.2 by Associate II
  • 3018 Views
  • 6 replies
  • 0 kudos

when getting ADC value, RMS processing is necessary needed?

Hello, I am using LO31K6 for sensoring two ADC channels by DMAWhen I wish to get trustable voltage value, Do I have to apply Root Mean Square to these ADC value?for example, < Instead directly get ADC value from DMA buffer[n] and treat as it is true ...

DU2 by Associate II
  • 1355 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F407 _ Packet transfer

Hi Team,How to transfer huge data through UART interface , is it any method or procedure to achieve. Brief description: Quectel module is been used, data of 80kb transported from AWS server to Quectel module.We need to identify the fastest and effici...

SS_135 by Associate II
  • 1488 Views
  • 2 replies
  • 0 kudos

stm32f446re nucleo board bit band ALIAS range

I have few doubts as follows:1. Each MEMORY MAPPED ADDRESS is how many bytes wide? 1 or 4 bytes (I think it as 1 byte).2. The ST datasheet for stm446xx says the SRAM is of 128Kb size then,start and end addresss is 0x20000000 to 0x2001FFFF but, bit ba...

Disha by Associate II
  • 2703 Views
  • 5 replies
  • 1 kudos

How to write protect STM32L4RZI internal flash

Hi!I'm trying to lock internal flash on STM32L4RZI  MCU from writing, to disallow software to write on itself.I use ST-Link utility, and when I lock at least one sector(In option bytes window), The flash is erased and then lock the wanted sector. I t...

SReef.1 by Associate
  • 1112 Views
  • 1 replies
  • 0 kudos

Resolved! Pin definitions on H7 MCU

On PIN/BALL defintion table of H7 MCU datasheet, these are a lot of alternate function pin names, such as TIM15_BKIN, TIM15_CH1N. Where can I find the detail describtions for these pin names?

JZou.2 by Associate II
  • 1485 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.