STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have a question about P-NUCLEO-USB001.

What I want to implement is to control the role of the module between host and consumer, when modules are connected to each other. Is it possible with programming ?If impossible with this module, what module can I use to implement that task ? Thank y...

HJin.2 by Associate
  • 1097 Views
  • 1 replies
  • 0 kudos

Resolved! Power Consumption by GPIO.

I am using STM32F779NI for my project.https://www.st.com/resource/en/application_note/dm00315319-stm32-gpio-configuration-for-hardware-settings-and-lowpower-consumption-stmicroelectronics.pdf Section 6.1 of above pdf states that unused input GPIO sho...

A3 by Associate III
  • 2428 Views
  • 2 replies
  • 0 kudos

Resolved! Only 4 Bits for Interrupt priority (NVIC STM32H743) ?

Hi,the IPR bit assignment in 'PM0253 Rev 5 p.189' tells me that a number of bits [n-1:0] are read as zero and ignore writes.At this point n isn't 'n = m MOD 4'.Obviously n is 4 because i can write only the four upper bits and bits [3:0] stay at zero....

DFuchs by Associate III
  • 2403 Views
  • 2 replies
  • 1 kudos

STM32F7508 change RTC after initialization

I believe I am doing something wrong. I read that to re-write to the RTC I will need to:1. Write ‘0xCA’ into the RTC_WPR register.2. Write ‘0x53’ into the RTC_WPR registerI found a function in the RTC file that is:#define __HAL_RTC_WRITEPROTECTION_DI...

DElli.1 by Associate III
  • 1175 Views
  • 1 replies
  • 0 kudos

I want to use the VCP capability for debugging.

I'm using the NUCLEO-303K8 board but I have the STM link/v2 and v3 to use too if that works better. I'm working inside the STMCubeIDE. The documentation that you can call up from within the application doesn't look like it matches the application, wh...

CArena by Associate II
  • 1906 Views
  • 1 replies
  • 0 kudos

How to implement VC0706 camera to STM32F4?

There are plenty of codes about VC0706 camera + Arduino. I tried the sample on Arduino and it worked pretty well. But I need to make this project with STM32. Any ideas how to implement and code VC0706 with STM32?

y.arikok by Associate II
  • 1435 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.