STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 OpAmp Differential Strain Gauge Bridge Input

Does anyone know if the PGA OpAmp in the STM32 has the ability to interface with a differential input - like a Strain Gauge Wheatstone bridge?  I'm not convinced its going to work because my signal is going to swing +/-50mV, and the OpAmp does no loo...

MIPI DSI not working on STM32U5

Hi,I have an issue on MIPI Display with our custom board, information as below, Core: STM32U599NJH6Frame Buffer Address: 0x200D0000 (Internal SRAM)MIPI Driver : ST7797Resolution: 400*400Reference example : STM32Cube_FW_U5_V1.6.0\ STM32U5x9J-DK\ DSI_V...

CharlieCHEN_0-1745985534542.png

Resolved! SIL 2 micrcontroller requirement

Hi, We are working on railway projects where we are looking for SIL 2 microcontroller. As per our analysis we found out that we need to integrate the X-CUBE-STL package to make it to SIL 2compliance. And we have found out that it should have supporte...

rajath by Associate II
  • 4280 Views
  • 13 replies
  • 3 kudos

Open web server data for B-U585I-IOT02A

Hello,I updated my development kit with the example IOT_HTTP_WebServer from the example selector in STM32 IDE. Then I needed to upgrade the firmware on wifi module, which seemed to work. I think I can connect to wifi, but I cannot open a webpage when...

GTanova by Associate III
  • 1080 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U5G9ZJT6Q: three displays (two SPI and one 24 RGB)

Hi, good morning to all. I'm in the process to design an application based on STM32U5G9ZJT6Q. My first question, please, is: is it possible to have this STM32 drive three different displays, and possibly have TouchGFX manage the whole three ?In my ca...

Matbonny by Associate III
  • 1921 Views
  • 5 replies
  • 0 kudos

STM32H735-DK LWIP pbuf assertion issues

I've been struggling with a variety of issues with FreeRTOS/LWIP/DHCP/MDNS, before I've even got to implement my application code (which will be a UDP app). I've read all of the documents that have been linked in the forums, I've gone through the off...

i2pi by Associate II
  • 1352 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.