2025-05-05 7:29 AM
Hi,
We are working on railway projects where we are looking for SIL 2 microcontroller.
As per our analysis we found out that we need to integrate the X-CUBE-STL package to make it to SIL 2compliance. And we have found out that it should have supported MCU's. As per our analysis the STM32H5 and STM32H7 series supports X-CUBE-STIL package.
So, we wanted to know are the safety certified libraries available in this package to make it as SIL 2 compliance. Also, can you suggest if there are any SIL 2 certified microcontrollers available.
Regards,
Rajath
Solved! Go to Solution.
2025-05-09 2:29 AM
SIL2 safety functions can be implemented with X-CUBE-STL on all listed devices; the necessary libraries are included in X-CUBE-STL. Technical support for this is handled not via this public community, but by the office with which you conclude the NDA.
Regards
/Peter
2025-05-05 8:32 AM
Welcome @rajath, to the community!
Yes, certified libraries are included in the software package.
To access the software, however, you must first conclude an NDA (Non-Disclosure Agreement) via your local distributor or local office of STMicroelectronics.
Good luck!
/Peter
2025-05-06 10:15 PM
Hi @Peter BENSCH,
Thank you for the quick response. May I know this software is free of cost or do we need to purchase the license to access this software?
Also, could you please confirm STM32H5 series supports X-CUBE-STL, or could you please suggest any other microcontroller which supports SIL 2 and have safety certified libraries.
Regards,
Rajath
2025-05-07 12:36 AM
If you have agreed an NDA, the software package X-CUBE-STL can be used free of charge and without a licence.
STM32H5 of course also supports the STM32H5, details and further microcontroller families can be found in the X-CUBE-STL safety manuals (don't forget to open the complete list of documents by clicking 'Load More' several times or 'Expand all categories'.
2025-05-07 1:13 AM
Dealing with projects requiring SIL-2, I suggest a Cortex R device. Preferably a dual-core lockstep configuration.
And from experience, I would highly recommend to consider an off-the-shelf ECU fulfilling this requirements.
2025-05-07 4:17 AM
ST already has some Cortex-R products? https://www.eenewseurope.com/en/st-plans-integrated-automotive-microcontroller-line/
2025-05-07 4:33 AM
One that note, not recommending one vendor or another ...
There are significant follow-up choices to make regarding a controller for a SIL-2 project.
One is the choice of a realtime OS - excluding an attempted bare-metal implementation (most likely to become a development and/or maintainance nightmare).
While there are free options (like FreeRTOS), they will imply higher costs downstream, because basically the whole project software must pass the certification.
Some pre-certified professional options (e.g. SafeRTOS) avoid a lot of this hassle, but come at relatively high initial costs.
And lastly, all those certifications (of either option) are bound to a toolchain. A replacement of this toolchain or even a major update will require a renewed certification process. With commercial safe RTOS variants one is usually bound to the vendor's choice, as RTOS and toolchain are pre-certified in tandem.
2025-05-09 12:34 AM
Hi @Peter BENSCH,
Thank you for the response.
After doing the thorough analysis on the microcontroller selection below part numbers are suitable for our application requirement both w.r.t Hardware and Software requirements.
STM32F469BI, STM32F469II, STM32F479BI, STM32F479II
STM32F765BI, STM32F767II, STM32F769II, STM32F779II
STM32H743ZIT6, STM32F769BI, STM32F412xE
For confirming the particular part number for our requirement, could you please confirm the above part numbers supports SIL 2 and also confirm that these part numbers are X-CUBE-STL supported, and safety certified libraries are included.
Regards,
K Rajath
2025-05-09 2:29 AM
SIL2 safety functions can be implemented with X-CUBE-STL on all listed devices; the necessary libraries are included in X-CUBE-STL. Technical support for this is handled not via this public community, but by the office with which you conclude the NDA.
Regards
/Peter
2025-05-09 2:33 AM
Thank you, Peter, for the confirmation.
Could you please let us know where can we find the NDA guidelines document so that we can go through? Should we check with the local distributor regarding this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.