2025-04-29 9:06 PM - edited 2025-04-29 9:08 PM
Hi,
I have an issue on MIPI Display with our custom board, information as below,
Reference example : STM32Cube_FW_U5_V1.6.0\ STM32U5x9J-DK\ DSI_VideoMode_SingleBuffer
I have noticed that example code is the same MIPI command and also LTDC timing as mine.
And I set as the same ,but still not display anything. So I checked few things,
If it is correct of my understanding, LP mode is for CMD configuration on level ~1.2V, HS mode is in data transfer for display on level ~200mV.
But as my measure, either same polarity or always on level 1.2V.
Is there anything I missed?
Any help will be appreciate~
Thanks.
2025-05-04 6:34 PM
Hi,
Is there anyone can help?
Thanks.
2025-06-10 1:13 AM
Since you did not mention the panel model hard to guess. Some LCD's need specific I2C commands to get them working and it's often not documented. Perhaps contact the supplier/manufacturer ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.