STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Procedures] How to use example codes : STM32Cube_FW_H7

Hi​I'm currently using STM32H743 and would like to try out example codes from STM32Cube_FW_H7.​Desktop\STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\LwIP\LwIP_UDP_Echo_Client​There were files in above directory.EWARMIncMDK-ARMSrcSW4STM...

SHong.5 by Associate II
  • 3347 Views
  • 5 replies
  • 0 kudos

Does the Nucleo STM32G431 have a bug with the I2S (receive)?

I am using the latest versions of STM32CubeIDE and updated firmware for STM32G431. I am trying to setup the Nucleo STM32G431 with I2S master for a microphone with DMA in circular mode, very similar to what "YetANotherElectronicsChannel" did in this v...

evenlund by Associate III
  • 5618 Views
  • 13 replies
  • 0 kudos

Resolved! Issue in debug mode when use Uart

Hello,I'm creating application with STM32F072, with ADC DMA, USB, Timers and Uart.Last one is used to communicate with PC but i verify a strange behavior.First of all general information:generating this software with STM32cubeMx. using IDE openstm32p...

AT.1 by Associate
  • 2672 Views
  • 2 replies
  • 0 kudos

ADC self calibration

​Hello,I am using STM32L471QE.​Please tell me how to calculate CALFACT_S and use it for ADC self calibration.I confirm that ADC1_CALFACT in CALFACT_S is 0x3A or 0x3B.I want to know how much [CALFACT_S] affects accuracy.Please let me know if there is ...

STaka.3 by Associate
  • 2916 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO output is running slower than clock frequency

HiI'm trying out stm32h743 now, and try to make output signal from GPIO.I've set same frequency on F429 & H743 with same code. However, The the signal much slower(longer) in H743.F429 400nsH743 4000ns (well... my purpose is to shorten the l...

0693W000005Ci8hQAC.png 0693W000005Ci8IQAS.png
SHong.5 by Associate II
  • 1496 Views
  • 2 replies
  • 0 kudos

Resolved! Synchronize Timer 1 and Timer 8 on STM32F446RE

Hi,I'd like to run synchronous PWMs on TIM1 and TIM8 of an STM32F446RE. I use TIM2 to trigger both timers.My setup:Master: TIM2MSM bit is setTRGO = Enable bit (CNT_EN)Slaves: TIM1 and TIM8Slave mode = Reset modeTrigger source = ITR1I appended my Cube...

STM32F429 bank swap for OTA update

HiFor a project I am using a STM32F429ZITx and need to implement OTA functionality. With single bank chips I have previously put the update into the free part of the flash, then copied it over and restarted.With 2 banks I came as far as erasing the u...

CKnez.1 by Associate II
  • 1075 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.