2020-11-24 11:15 PM
Hi
I'm currently using STM32H743 and would like to try out example codes from STM32Cube_FW_H7.
Desktop\STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\LwIP\LwIP_UDP_Echo_Client
There were files in above directory.
Since I'm using Atollic TrueStudio, so I ran .project in SW4STM32.
However, after I BUILD PROJECT, the message "Info: Nothing to build for STM32H743I_EVAL". I tried to import src, inc folders, but it seems like it doesn't compile.
Can anybody help me out with this?
Thanks in advance
Solved! Go to Solution.
2020-11-26 6:12 PM
> Since I'm using Atollic TrueStudio, so I ran .project in SW4STM32
Unfortunately SW4STM32 projects don't build as is with Atollic. You have to import (convert) them. See the Atollic documentation.
After conversion, fix some small issues - if I remember correctly, make the project to use the original linker script (.ld file) instead of auto-created.
-- pa
2020-11-26 6:12 PM
> Since I'm using Atollic TrueStudio, so I ran .project in SW4STM32
Unfortunately SW4STM32 projects don't build as is with Atollic. You have to import (convert) them. See the Atollic documentation.
After conversion, fix some small issues - if I remember correctly, make the project to use the original linker script (.ld file) instead of auto-created.
-- pa
2020-11-27 12:07 AM
Hello @SHong.5 ,
You can use STM32CubeIDE (all-in-one multi-OS development tool) and follow the guide to import Cube projects from SW4STM32 or TrueSTUDIO to STM32CubeIDE:
Imen
2020-11-27 12:42 AM
@Imen DAHMEN According to UM2579 that you have linked, it is not possible to convert multicore SW4STM project to CubeIDE.
The guide says:
• It is not possible to convert to STM32CubeIDE a mutlicore project created in System Workbench for STM32
And @SHong.5 is using dualcore STM32H7.
Regards,
2020-11-27 1:43 AM
Hi @Frak.1 ,
That sentence is a bit old, the guide is old and probably needs updating.
I recommend you to follow the AN5361 STM32H7 guide for import, in Section 2.5 Import a project from the STM32CubeH7 MCU Package.
Imen
2020-11-27 2:58 AM
Good to know, thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.