STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H755ZI SPI / Proper way to receive data

Hi everyoneI'm currently working with the STM32H755ZI SPI1 peripheral. I'm using low level driver to read 2 bytes of data. I'm transmitting 2 dummy data bytes (0xFF) in order to get some response from the SPI slaves. Most of the time, the receive wor...

DSchl.1 by Associate III
  • 7031 Views
  • 11 replies
  • 0 kudos

Hi i am using nucleo L073Rz board , how do we authenticate a user application bin file flashed in to a board from iap is the correct bin and move on to run.

The problem is crc used in iap for transferring the bin file is to only check for errors during the transfer process , however i dont want any random bin files to be flashed into the flash or executed from it, only certain signed bin files need...

svii by Associate III
  • 1789 Views
  • 3 replies
  • 0 kudos

__disable_irq() in ISR possible?

Hello,I have a global variable, wich is accessed by multiple ISRs. Can I safely disable and re-enable the interrupts within an ISR using __disable_irq() and __enable_irq()?Or is there a more elegant way of protecting the variable access?best regards,...

STM32L4 serial communication doesnt work!

hey,i have an STM32L432KBU6 and i want to serial communicate with my chip. I connected the SWCLK, SWDIO and the SWO pin and followed a couple tutorial on youtube but i just cant get the Serial communication done. i just want to open serial monitor li...

OTosu.1 by Associate II
  • 1385 Views
  • 2 replies
  • 0 kudos

I am unable to configure CAN in STM32L476VG Discovery board. I wanted to develop an application which sends CAN message and receives CAN message. I enabled 2 interrupts CAN1_TX_Interrupt, CAN1_RX0_Interrupt. I selected Normal Mode only .

When debugging I found that MX_CAN1_Init() is not getting initialized, inside this code HAL_CAN_Init() is blocked by a while loop.That blocking iteration is as follows/* Get tick */ tickstart = HAL_GetTick(); /* Check Sleep mode leave acknowledge */ ...

RahulR by Associate II
  • 1596 Views
  • 2 replies
  • 0 kudos

MCU locks up the moment a relay closes. Are there any tips to stabilize / make the MCU less sensitive to external noise?

We have a board with a STM32G071RBT6. The MCU is controlling a mechanical relay that breaks mains voltage (230V). When the relay closes, this causes the MCU to hiccup in rare occasions: either the core locks up and the WDI resets it, or a NMI excepti...

AEste.1 by Associate
  • 952 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.