STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Use of Odd Parity in USART1 Configuration -- stm32L452RE uC

Hi--I/m pretty stumped. I am trying to implement a odd parity configuration for USART1 in an stm32L452RE micro. I've confirmed without parity the usart behaves as expected at the needed baud. When i introduce parity into the code and sniff the data o...

rsoc by Associate III
  • 2070 Views
  • 2 replies
  • 0 kudos

Resolved! HAL_SPI_TransmitReceive_DMA read before write

HiI'm using the HAL_SPI_TransmitReceive_DMA to write to an external Flash. On a delte command for the external flash I need to wait for until the busy flag of the flash is zero. So I use this function to check the busy flag. spi_read(&command, sizeo...

dominik by Senior
  • 1706 Views
  • 4 replies
  • 0 kudos

Conflict with Timer8 and ADC1 interrupts

Hello everyone, I use a STM32F407VET6 MCU board and I'm trying to implement a Timer 8 Interrupt, every 5u sec. In my code, I also use an ADC interrupt, for ADC conversion purposes. I thought that these 2 interrupts are independent. I observed that w...

0693W000007E6cvQAC.jpg 0693W000007E6cMQAS.jpg 0693W000007E6biQAC.jpg
KS.5 by Associate
  • 3316 Views
  • 4 replies
  • 0 kudos

Cannot erase/program flash using jtag

HiI've set the jtag pins in my code to analog input (non intentionally) .While I was able to connect to Device (STM32H743) after I managed to erase the flash option bytes (with mass erase) using j-link stm32 tool (No St-Link option or SWD for me on ...

deckhard by Associate III
  • 1597 Views
  • 3 replies
  • 0 kudos

STM32L476: Code runs into Reset Handler if Interrupts get activated although no Interrupts are triggered

Hi,I have some code running on a Nucleo-STM32L476 which keeps running into the Reset Handler. But this does not cause a boot loop, instead the code just gets stuck there (the PC register points to the first line of assembler of the reset handler).I m...

Resolved! Problem READING PIN

Hello everyone, I am trying to read one pin with the HAL libraries, but i can not. This is my configuration:  1) I want to read the "BUTTON" pin ( PB3/PB4/PB5/PB6 ) 2 I am doing this:  GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GP...

0693W000007E72oQAC.jpg
NFahi.1 by Associate II
  • 1834 Views
  • 3 replies
  • 0 kudos

Resolved! correct use of GPIO_Analog

Hello. I have a question about the correct use of GIPO_Analog.wanted to read this value.I also want to know if the value can vary between 0 to 4095 as when the ADC is used.am I using an MCU that I use Nuclo-F446RE?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.