2021-01-29 8:32 AM
Hi,
I have some code running on a Nucleo-STM32L476 which keeps running into the Reset Handler. But this does not cause a boot loop, instead the code just gets stuck there (the PC register points to the first line of assembler of the reset handler).
I modified the Systick to read a hardware-based timer so it works without interrupts. But the Code shows the same behaviour when using the default Systick implementation.
The conditions under which the reset handler gets called are really weird:
Does anyone have an idea why this happens? I essentially want to have interrupts disabled in the first firmware layer and have them enabled in the second layer. This works if I execute them individually, but if i execute them after another I cannot enable interrupts at any point.
Thank you.
2021-01-29 9:11 AM
Hello
It seems that Systick IRQ handler is missing or is not linked.
2021-01-29 9:56 AM
Yeah, that could be the case because it is not in the assembler code (I am using the default Systick IRQ Handler). In fact the ADC1_2_IRQHandler is the only IRQ Handler in the assembler code, but it is basically empty (consisting of one assembler instruction). I tried including it in the startup code (I am using the default file from CubeMX) with the following:
.word HAL_SYSTICK_IRQHandler
.weak HAL_SYSTICK_IRQHandler
.thumb_set HAL_SYSTICK_IRQHandler,Default_HandlerThis did not work (I also tried it without "HAL_" in front of it, but that did not work either).
On the other hand, the second firmware layer also does not have the Systick IRQ Handler in its assembler code. It has an UART, RNG, TIM and ADC1_2 IRQ Handler, but thats due the CubeMX settings I made. And this firmware works fine with interrupts, so why does the other one not work?
2021-01-29 12:10 PM
So basically even a blinky doesn't work... Make a copy of the project and strip it down until you get it working. That includes stripping off the HAL and CubeMX generated junk.
Just some ideas... To what value is the stack pointer initialized? What's with the use of float/double types and FPU hardware?
2021-01-29 1:43 PM
What is " first firmware layer" and "second layer"?
JW
2021-02-01 12:10 AM
I have two binaries in the memory where the first binary jumps into the second binary when it has finished its execution. Basically the first firmware layer is similar to a bootloader and the second one is the application.
2021-02-02 3:03 AM
I now found that it is indeed the SysTick IRQ causing this. But the handling of the IRQ is weird: By default a proper SysTick Handler is linked in the startup file, but this just gets ignored. I found that the code just ignores anything that is linked as the first Handler.
These are the default Handlers for SysTick:
.weak SysTick_Handler
.thumb_set SysTick_Handler,Default_HandlerHere the executable just ignores my changes if I exchange the SysTick_Handler, but if i switch the Default_Handler then it gets called properly. So my solution is to just set the SysTick_Handler to the second Handler like this:
.weak SysTick_Handler
.thumb_set ShouldBeNeverCalled,SysTick_HandlerDoes anyone have an idea why the first entry gets ignored? By the way I also checked the ICSR register, but it was also displaying incorrect information (it said IRQ 15 - DMA1_Channel5_IRQn - was the interrupt causing this).
2021-02-02 6:53 AM
How do you manage the vector tables/VTOR when going from "one layer" to the "other layer"?
JW
2021-02-02 8:54 AM
I set the SCB->VTOR accordingly before jumping to the next layer. But this problem is unrelated to the jumping because this problem only exists in the first layer, before the code jumps.
But I am fine with using the workaround, I am just curious why the first entry is ignored.
2021-02-05 5:50 AM
The "first entry" is the default handler and normaly is a branch instruction to the same address.
This default handler is defined as weak
In case there is another function defined with the same name , the linker will links the handler without weak symbol.
So the "first entry" will never be called , in case the handler is defined in another module.
To debug startup file note that the compiler's optimisation level should be at minimum ....Oo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.