2021-02-03 5:12 AM
Hi
I'm using the HAL_SPI_TransmitReceive_DMA to write to an external Flash. On a delte command for the external flash I need to wait for until the busy flag of the flash is zero. So I use this function to check the busy flag.
spi_read(&command, sizeof (command), &SPI_RX_BUFFER, 2);
if ((SPI_RX_BUFFER[1] & 1) == 0)
return true;
else
return false;void spi_read(const void *txdata, size_t txsize, void *rxdata, size_t rxsize)
{
HAL_GPIO_WritePin(Flash_NSS_GPIO_Port, Flash_NSS_Pin, GPIO_PIN_RESET);
//reset the TX_RX complete Indication
SPI_TXRX_Complete (true, false);
SPI_TXRX_Status_Complete (true, false);
HAL_SPI_TransmitReceive_DMA (&hspi3, (uint8_t *)txdata, (uint8_t *)rxdata, rxsize);
}The problem is, that the RX of the DMA is not ready when I check the busy flag:
SPI_RX_BUFFER[1] & 1
How can I fix this issue?
Solved! Go to Solution.
2021-02-03 10:58 PM
It's running, problem was that with high optimization debugger I got wrong and inpossible results. I changed the icf file to a bigger range ange disabled the optimization, now it works like it should.
2021-02-03 11:38 AM
Observe the communication on the SPI pins using logic analyzer.
JW
2021-02-03 10:58 PM
It's running, problem was that with high optimization debugger I got wrong and inpossible results. I changed the icf file to a bigger range ange disabled the optimization, now it works like it should.
2021-02-05 6:06 AM
If your MCU has a data cache, the observed behaviour at high optimzation could be due to cache incoherency.
2021-02-05 7:07 AM
I changed my icf file to a 1 image Debug config, now I can debug without optimization
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.