STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Are these Memory segmentation Problems even possible?

Hi, I am new to using 32 bit microcontrollers and have been using 8 bit controllers previously. In my 8 bit controllers I had several uint8_t and uint16_t variables.Does a 32 bit microcontroller access 4 bytes of data in memory at once? If yes, can t...

PPULA.1 by Associate II
  • 1464 Views
  • 1 replies
  • 0 kudos

Resolved! STSPIN32F0 And STSPIN32F0A

I **** to buy  STSPIN32F0A,but the IC's label is the STSPIN32F0. So how to identify them by the label of the IC. Thank you very much

Wzong.1 by Associate III
  • 1235 Views
  • 1 replies
  • 0 kudos

Resolved! How to disable PWM output properly?

Hello,My timer PWM channel is connected directly to a mosfet driver. By using TIM_Cmd(TIM2, DISABLE);it puts the output at high level. I tried to use TIM_DeInit(TIM2); but it generates an additional pulse in the output ( I count the each PWM pulse in...

JJohn.3 by Associate II
  • 5030 Views
  • 4 replies
  • 0 kudos

Code stuck in SD_FindSCR Function

Hello,I use stm32f765BITx processor and SDMMC (SD 4 bits Wide bus ), sometimes code is stopping at SD_FindSCR function in stm32f7xx_hal_sd.c library. This event is happening random.Exactly, the place where code stopped at SD_FindSCR function,while(!_...

LDesa.1 by Associate II
  • 4120 Views
  • 6 replies
  • 0 kudos

Resolved! Setting up TIM1 in Encoder Mode

Hi,I am trying to setup the TIM1 of the STM32F410CBT microcontroller so that TIM1->CNT can measure Channel A and Channel B of a Quadrature Encoder Interface of a motor (the Encoder's datasheet is here, and it came attached with this motor here). I ha...

0693W000007DhROQA0.jpg
RrW1 by Associate III
  • 8069 Views
  • 4 replies
  • 0 kudos

Resolved! STM32G070RB Vbat Data sheet error

According to the data sheet, sec 3.13.3 says the VBAT voltage is measure by the ADC as VBAT/3, or one third Vbat.using : uint64_t volt = (uint64_t)(((uint64_t)3300U*adc_result)/(uint64_t)4095U);I get 2/3 VbatChanging to uint64_t volt = (uint64_t)(((...

MEder by Associate III
  • 3266 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.